2017-08-31 7:23 PM
Hi,
I'd like to buy STM32F429I-DISC1 kit for study. but I can't find STM32F429I-DISC1's specification what I mean is such a memory map and detail connectives information with memory map.
How do I get
STM32F429I-DISC1's detail connectives information with memory map?
Should I have to just guess with general information from
?Or can I find STM32F429I-DISC1's detail specification to fit by itself?
#memory-map #stm32f429i-disc1Solved! Go to Solution.
2017-08-31 8:24 PM
Not sure these things need to be guessed, the schematic and chip docs tend to be fairly definitive.
The Reference Manual for the chip is also quite useful
The SDRAM on the STM32F429I-DISCx board is at 0xD0000000 in the memory map, 8MB, so 0xD0000000..0xD07FFFFF
2017-08-31 8:24 PM
Not sure these things need to be guessed, the schematic and chip docs tend to be fairly definitive.
The Reference Manual for the chip is also quite useful
The SDRAM on the STM32F429I-DISCx board is at 0xD0000000 in the memory map, 8MB, so 0xD0000000..0xD07FFFFF
2017-08-31 10:31 PM
Original thread I had on the board
https://community.st.com/0D50X00009XkgXjSAJ
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.