2018-03-26 3:23 PM
I am using STM32F7(216MHz). When I test input capture of TIM2 and TIM11, rising edge interrupt was missimg some time. The callback function is not call by interrupt at the ratuo about 1 of 100. Input signal frequency is 450kHz.
What should I do to captue input signal without missing interrupt function call.
Thanks.
#stm32f7 #interrupt #maximum-frequency #input-capture2018-03-26 4:52 PM
the IO clock is set to slow medium or fast. that is double your maximum frequency.
the pin has to go up and be clocked in, and it has to go down and be clocked in..
your maximum frequency is half the IO pin clock frequency.
2018-03-26 5:26 PM
At higher frequencies consider
a) Counting pulses over an integration period
b) Use input prescaler to measure the time over 8x periods
c) Use DMA to capture time stamps, and decimate interrupt load by defining buffer length for samples.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.