2016-11-09 12:30 PM
How much I can put on Vref without lossing bit?
I can read 8 bit without nise (12 bit is noisy) when the Vref is 3.3V. however, my sensor show maximum 12 (decimal). I wan to get more resolution. Therefore I want to change Vref. What is minimum Vref without lossing data or adding noise? can I coonect it to 0.15 V? #adc2016-11-09 1:26 PM
Wouldn't that be in the Data Sheet? Usually such things only allow a small differential between VDD/VDDA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.