2022-02-03 10:15 PM
I have a PCA design which I'd like to support both devices with min configuration changes in the PCB dependent on the fitted device. I've made provision VACP1/2 options - either CAP or 0R resistor to VSS.
2022-02-04 6:50 AM
You can get a reasonable answer from this using CubeMX.
They are quite different chips. Unlikely for the code to be compatible even if the footprint can be managed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.