2009-10-06 10:24 PM
Weird Boot up
2011-05-17 4:25 AM
Hi everybody!
I've got a wierd problem with my board. Im using Crossworks 1.7, and the problem is that the first time i upload the program to flash it works properly but when the second time i try to upload i get the message ''Loader is not a libmem RPC loader''. when i upload again it works to upload but the program doesnt work properly. The timers and adc wont start up. The thing i can do to make it work again is to unplug the power supply and upload again. but the second time i upload its the same thing all over again. I hope you can help me. Regards Niklas Cooke2011-05-17 4:25 AM
Have you asked Rowley (the makers of Crossworks)?
In my experience they are helpful and come back with solutions to problems reasonably quickly. I have had problems with debugging / subsequent downloads when enabling copy-protection or using the debug pins for GPIO. But that should not come as a surprise. Hope this helps, DanishWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.