2021-03-16 1:10 AM
Hi all,
I'm learning about low power modes , and I'm testing the RTC wakeup timer function.
Datasheet talks about to set the IRQs for WakeUp timer on EXTI(IRQ 19) and NVIC(IRQ 3), but I tested in my code, with and without set these IRQs and the wakeup timer works well in both cases.
What I'm doing wrong?
The MCU is a STM32F3 family one.
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2021 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
uint8_t x;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void ClockInit(void)
{
//Queremos trabajar a 16MHz, con HSE y LSE
//Cambiamos el SYSCLK source a HSI
RCC->CFGR &= ~(RCC_CFGR_SW);
while((RCC->CFGR & RCC_CFGR_SWS));
//Para el PLL
RCC->CR &= ~(RCC_CR_PLLON);
while(RCC->CR & RCC_CR_PLLRDY);
//El cristal es de 8MHz, por lo que hacemos PLL x2
RCC->CFGR &= ~(RCC_CFGR_PLLMUL);
RCC->CFGR |= RCC_CFGR_PLLMUL_0;
//Enciende el HSE y espera a que HSE_RDY se ponga a 1
RCC->CR |= RCC_CR_HSEON;
while(!(RCC->CR & RCC_CR_HSERDY));
//Hacemos que el source del PLL sea el HSE/PREDIV
RCC->CFGR |= RCC_CFGR_PLLSRC_HSE_PREDIV;
//Encendemos el PLL
RCC->CR |= RCC_CR_PLLON;
while(!(RCC->CR & RCC_CR_PLLRDY));
//Hacemos que el APB1 sea de 16MHz
RCC->CFGR &= ~(RCC_CFGR_PPRE1);
//El valor de LATENCY se debe ajustar en función de la velocidad del SysClock. 0 para 16MHz
FLASH->ACR &= ~FLASH_ACR_LATENCY;
//El SYSCLK es el PLL
RCC->CFGR &= ~(RCC_CFGR_SW);
RCC->CFGR |= RCC_CFGR_SW_1;
while((RCC->CFGR & RCC_CFGR_SWS_0) && !(RCC->CFGR & RCC_CFGR_SWS_1));
//----------------------Programamos el LSE-------------------------------
//Para poder programarlo se debe activar PWR_CR_DBP
PWR->CR |= PWR_CR_DBP;
//Habilitamos el reloj RTC
RCC->BDCR |= RCC_BDCR_RTCEN;
//Seleccionamos LSE como source
RCC->BDCR &= ~(RCC_BDCR_RTCSEL);
RCC->BDCR |= RCC_BDCR_RTCSEL_0;
//Encendemos el RTC y esperamos a que esté listo
RCC->BDCR |= RCC_BDCR_LSEON;
while(!(RCC->BDCR & RCC_BDCR_LSERDY));
//Bajamos el bit de PWR_CR_DBP
PWR->CR &= ~(PWR_CR_DBP);
SystemCoreClockUpdate();
SysTick_Config(SystemCoreClock/1000);
}
void GpioInit(void)
{
RCC->AHBENR |= RCC_AHBENR_GPIOAEN;
GPIOA->MODER &= ~(GPIO_MODER_MODER11);
GPIOA->MODER |= GPIO_MODER_MODER11_0;
}
void SetWakeUpTimer(uint16_t segundos)
{
//EXTI->IMR |= EXTI_IMR_IM20;
//EXTI->RTSR |= EXTI_IMR_IM20;
//EXTI->FTSR &= ~(EXTI_IMR_IM20);
//NVIC_EnableIRQ(3);
PWR->CR |= PWR_CR_DBP;
RTC->WPR = 0xCA;
RTC->WPR = 0x53;
RTC->CR &= ~(RTC_CR_WUTE);
while(!(RTC->ISR & RTC_ISR_WUTWF));
RTC->WUTR = segundos;
RTC->CR &= ~(RTC_CR_WUCKSEL);
RTC->CR |= RTC_CR_WUCKSEL_2;
RTC->CR |= RTC_CR_WUTIE;
RTC->CR |= RTC_CR_WUTE;
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
//SystemClock_Config();
/* USER CODE BEGIN SysInit */
ClockInit();
GpioInit();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
SetWakeUpTimer(3);
PWR->CR |= PWR_CR_CSBF;
PWR->CR |= PWR_CR_CWUF;
RTC->ISR &= ~(RTC_ISR_WUTF);
GPIOA->BSRR |= GPIO_BSRR_BS_11;
HAL_Delay(50);
GPIOA->BSRR |= GPIO_BSRR_BR_11;
HAL_Delay(50);
GPIOA->BSRR |= GPIO_BSRR_BS_11;
HAL_Delay(50);
GPIOA->BSRR |= GPIO_BSRR_BR_11;
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
PWR->CR |= PWR_CR_PDDS;
__WFI();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.