2024-07-03 1:21 AM
Hi.
I'm using STM32F303RCT6 now.
Is it possible to set one pin vss using gpio settings?
If so, is there a specific pin?
If you have any question, ask me.
Thank you.
2024-07-03 1:23 AM
Hello,
Not sure what do you mean by this:
Is it possible to set one pin vss using gpio settings?
If so, is there a specific pin?
Could you please clarify?
2024-07-03 4:43 PM
There are 4 Vss pins in MCU : STM32F303RCT6.
I want to add 1 Vss pin in there.
How can i add it?
Is it impossible?
2024-07-03 6:09 PM
@giwonKIM wrote:There are 4 Vss pins in MCU : STM32F303RCT6.
I want to add 1 Vss pin in there.
How can i add it?
Is it impossible?
You're still not very clear on what you're trying to achieve?
You want to add 1 Vss pin to among the already 4 Vss pins to make 5 Vss pins? Or are you wanting to convert 1 of Vss pin to a GPIO?
2024-07-03 6:19 PM
Hi.
I'm trying to add 1 Vss pin to make 5 Vss pins.
2024-07-03 6:27 PM
And this extra Vss pin is supposed to do what?
2024-07-04 12:49 AM
I'm trying to add 1 Vss pin to make 5 Vss pins.
You didn't mention why you want to do that?! Do you have a PCB constraint and you have a GND layout that you are obliged to pass through a GPIO pin? if yes, which pin?
You need to provide more information about your case and be concise so we can help you efficiently.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.