cancel
Showing results for 
Search instead for 
Did you mean: 

VREFBUF enable for STM32L476VG not possible?

Merlin Ma
Associate
Posted on May 02, 2017 at 10:54

I am using a STM32L476VG (100 pin package, VREF+ not bonded to VDDA) for a mixed signal design. I planed to use the VREF+ as a 2.048V reference output. Currently there is no load on the VREF+ pin.

Unfortunately I always get a HAL_TIMEOUT while waiting for the VRR bit in the VREFBUF CSR register:

HAL_SYSCFG_VREFBUF_VoltageScalingConfig(SYSCFG_VREFBUF_VOLTAGE_SCALE0);
HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);
if (HAL_SYSCFG_EnableVREFBUF() != HAL_OK)
{
Error_Handler(ENVREFO_ERROR);
}�?�?�?�?�?�?

Also no voltage output is measureable at the VREF+ pin...

Do I miss something here? I tried to change the order or manually set the registers (without time-out) but no output at all.

Thank you for your help!!

Best regards,

Merlin

#analog #vrefbuf #reference #vref+ #csr
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Merlin Ma
Associate
Posted on May 04, 2017 at 10:40

For everyone having the same problem:

Enable clock for SYSCFG: Set bit 0 in RCC_APB2ENR before enabling the VREFBuffer.

View solution in original post

1 REPLY 1
Merlin Ma
Associate
Posted on May 04, 2017 at 10:40

For everyone having the same problem:

Enable clock for SYSCFG: Set bit 0 in RCC_APB2ENR before enabling the VREFBuffer.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.