2018-03-15 2:49 PM
Hello,
I will use this Cortex with both ADC and both DAC active.
The datasheet says the maximum (wort case) current required into Vref is:
220 uA for ADC and 220 uA for DAC.
I am going to apply the separate Vref with a shunt reference hence I need to calculate the pullup resistor. So I must know what is the maximum (worst case) current I must provide for Vref pin.
Is it 2x for ADC + 2x for DAC = 880 uA ?
Or less (as buffered inside the chip) ?
Or even more as the max current for DAC in the datasheet is for 'Standby mode, no load'. So should I increase the total Vref current still more (for Run mode and some load) ?
Thank you for any help.
Best regards
Robert
2018-03-16 12:22 AM
' The datasheet says the maximum (worst case) current required into Vref is 220 uA for ADC and 220 uA for DAC'
I think they are saying the minimum required to satisfy the internal circuits is 440uA in the worst case.
It could be lower on some batches but not always.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.