2009-03-03 10:34 PM
Virtual COM Port example
2011-05-17 4:05 AM
Hello,
I am using the Virtual COM Port example code as the basis of the firmware for a USB <-> ZigBee device made by the company I work for. Our previous design used an FTDI and so it seemed a perfect fit for minimal-change for our customers to begin with. However I'm having a lot of trouble with the reliability of the communications channel. I have found several threads on here which deal with improving the Virtual COM Port demo by using buffers, regulating when the endpoints become available etc. Basically I was wondering if anyone at ST had looked at these and perhaps produced an official improved Virtual COM Port demo? Regards, Daniel.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.