2009-11-28 1:43 AM
Virtual COM Port driver
2011-05-17 4:32 AM
In the download area there is a VCP Driver for Windows. For the moment, my application communicates by physical COM port not available at many new laptops. Therefore, my board already has a USB socket. As far as I understand, the STM32 app has to show a behaviour of a CDC.
Unfortunately, I did not find any application note or firmware example on how to program the enumeration and Rx/Tx of such CDC using the Std_PeriphLib.2011-05-17 4:32 AM
Dear Janvi,
Refer to ''STM32_USB-FS-Device_Lib'' :http://www.st.com/stonline/products/support/micro/files/um0424.zip
and then go to Project : ''\Project\Virtual_COM_Port''. Have a nice weekend, Cheers, STOne-32.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.