2019-11-10 12:10 AM
I am French.
There is now more than one week that I try, see youtube and some comments on forum. I need your experience for solving the initialisation of a "simple" PWM.
Thanks in advance.
Joël
here under my code. in the main I have launch : PWM1_CH3N_setup();
void PWM1_CH3N_setup(void)
{
// STM32F302R8
// Clock Frequency = SystemCoreClock = 64 000 000 Hz
// Period = 38000 - 1 = 37999
// Prescaler = (SystemCoreClock/38000) - 1
// Pulse = 190000;
// ClockDivision = 0
// Counter direction = Up
// for try I use 1hz
/* Set TIM1 clock source as internal clock */
LL_RCC_SetTIMClockSource(LL_RCC_TIM1_CLKSOURCE_PLL);
/* TIM1 clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_TIM1);
/* GPIO config */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOC);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOF);
GPIO_InitStruct.Pin = PF0_PWM38khz_Pin ;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_TIM1; // proposed by CUBE
HAL_GPIO_Init(PF0_PWM38khz_GPIO_Port, &GPIO_InitStruct);
GPIO_InitStruct.Pin = PC2_PWM38khz_Pin ;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF2_TIM1; // proposed by CUBE
HAL_GPIO_Init(PC2_PWM38khz_GPIO_Port, &GPIO_InitStruct);
/* TIM1 init function */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 64000;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 1000;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
/* Initialization Error */
error_data = 100 ;
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&TimHandle, &sClockSourceConfig) != HAL_OK)
{
/* Initialization Error */
error_data = 101 ;
Error_Handler();
}
if (HAL_TIM_PWM_Init(&TimHandle) != HAL_OK)
{
/* Initialization Error */
error_data = 102 ;
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 500;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&TimHandle, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
/* Initialization Error */
error_data = 103 ;
Error_Handler();
}
if (HAL_TIM_PWM_Start(&TimHandle, TIM_CHANNEL_3) != HAL_OK)
{
/* Initialization Error */
error_data = 104 ;
Error_Handler();
}
}
2019-11-10 2:07 AM
In debugger, read out and check/post the relevant GPIO and TIM registers content.
JW
2019-11-10 9:58 AM
here under the debug result register.
GPIO PC2
MODER1[bits 3-2] 0x3
AFRL2 [bits 11-8] 0x2
AFRH10 [bits 11-8] 0x6
AFRH11 [bits 19-16] 0x6
IDR2 [bits 2] 0x1
OSSPEEDR1 [bits 3-2] 0x00
-
-
GPIO PF0
MODER0[bits 1-0] 0x2
AFRL0 [bits 3-0] 0x6
OSSPEEDR1 [bits 3-2] 0x00
-
-
TIM 1
CR1 all bits = 0x00
CR2 all bits = 0x00
SMCR all bits = 0x00
DIER all bits = 0x00
SR UIF [bit 0] = 0x1 and all others bits 0x00
CCMR1_output all bits = 0x00
CCMR1_input all bits = 0x00
CCMR2_output all bits = 0x00
CCMR2_input all bits = 0x00
CCER all bits = 0x00
CNT all bits = 0x00
PSC [bits 15-0] = 0xFA00
ARR [bits 15-0] = 0x03E8
RCR [bits 15-0] = 0x0000
CCR1[bits 15-0] = 0x0000
CCR2[bits 15-0] = 0x0000
CCR3[bits 15-0] = 0x0000
CCR4[bits 15-0] = 0x0000
BDTR all bits = 0x00
DCR all bits = 0x00
DMAR all bits = 0x00
CCMR3 all bits = 0x00
CCR5 all bits = 0x00
CCR6 all bits = 0x00
OR all bits = 0x00
2019-11-10 10:19 AM
> GPIOC
> MODER1[bits 3-2] 0x3
We are talking about PC2, so would need to have a look at MODER2 (bits 5-4 of GPIOC_MODER).
Does this mean they are 0x0 ? Then they are set as In, not as AF - AF is 0x02. As I've said I don't use Cube so don't quite understand why, but maybe you want to check the values used for setting up PC2. Make sure, you fill in all fields of the GPIO_InitStruct, and/or zero it explicitly.
GPIOC_AFRL appears to be set properly, though. I don't know why did you post GPIOC_AFRH's bits - those two appear to map PC10+PC11 to SPI3SCK+SPI3MISO, isn't that what you intended to do?
GPIOF appears to be OK.
TIM has set ARR and PSC, but that's all - you need to have set CCRx for channel X to a value between 0 and ARR, CCMRx set for output compare/on of the PWM modes, channel output(s) enabled in CCER, and timer/counter enabled in CR1.CEN. Again, I don't use Cube so I can't decipher your code, but I'd perhaps check if TimHandle is set properly, as that appears to be a common denominator of all called functions except the function which sets the "timebase" i.e. ARR and PSC.
JW
2019-11-10 2:09 PM
JW,
I have check, MODER2 [bits 5-4] = 0x2. i think now PC2 is ok no?
yes, my SPI3 is set
I understand that the structure "sConfigOC" is wrong because the "sConfigOC.pulse = 500" not 0x0 .
Thanks, Joël
2019-11-10 2:20 PM
> I have check, MODER2 [bits 5-4] = 0x2. i think now PC2 is ok no?
Yes that's what's expected.
JW
2019-11-11 1:11 AM
I JW;
I have found with your questions , "&Timhandle" is wrong , I need to use "&htm1"
I have tested and now I have output on PF0 . This is that I need . I don't need PC2 . I have used PF0 and PC2 for tring only.
here under the final code for 38khz PWM that works.
void PWM1_CH3N_setup(void)
{
// STM32F302R8
// Clock Frequency = SystemCoreClock = 64 000 000 Hz
// PWN needed = 38000 hz
/* Set TIM1 clock source as internal clock */
LL_RCC_SetTIMClockSource(LL_RCC_TIM1_CLKSOURCE_PLL);
/* TIM1 clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_TIM1);
/* GPIO config */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOC);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOF);
GPIO_InitStruct.Pin = PF0_PWM38khz_Pin ;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_TIM1;
HAL_GPIO_Init(PF0_PWM38khz_GPIO_Port, &GPIO_InitStruct);
/* TIM1 init function */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 20;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 160;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
/* Initialization Error */
error_data = 100 ;
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
/* Initialization Error */
error_data = 101 ;
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
{
/* Initialization Error */
error_data = 102 ;
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 80;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
/* Initialization Error */
error_data = 103 ;
Error_Handler();
}
if (HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3) != HAL_OK)
{
/* Initialization Error */
error_data = 104 ;
Error_Handler();
}
}
Thanks you very much JW.
bye bye.
Joël
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.