2009-01-10 5:34 PM
Using Internal oscillator of STM32
2011-05-17 3:58 AM
is there any limitation or hurdle or bottle necks in using the internal crystal oscillator on STM32F103RB. This is a 64 pin TQFP package.
Also, if internal oscillator suffices the need of micro.. can i use the OSC-in and osc-out pin as remap for CAN_Rx and CAN_Tx. Pls guide with all possibilites. thanks and regards, nr_naik. wish u all @ ST family a happy and prosperous new year !2011-05-17 3:58 AM
I was wondering this as well if the internal RC oscillator (1% accuracy) is sufficient for accurate CAN performance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.