2018-04-04 8:08 AM
Is it possible to use the I2S_CKIN external clock source for SPI rather than come off the peripheral clock? From the reference manual it appears that this external clock is available as a source only when the SPI is in 'I2S Mode'. Is there a workaround? I am using an STM32F765. Thanks!
#i2s_ckin #spi2018-04-04 8:30 AM
>>
it appears that this external clock is available as a source only when the SPI is in 'I2S Mode'
OR an SPI Slave
2018-04-04 10:50 AM
Yes, that makes sense. Looking a little more closely at the reference manual, it looks pretty clear that an SPI Master clock can only be sourced from PCLK2 with a divider that is configured through the BR[2:0] bits in the SPIx_CR1 register. The I2SSRC bit in the RCC_CFGR register is stated to configure the source for I2S only.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.