2025-09-26 11:08 AM
Hi, we are developing a device which outputs display port over type-c and needs to sink power. Similar to Laptops when connected to hubs. The required power is less than 60W.
Im looking a for a suitable USB-PD implementation for this purpose. Can this be achieved using the USB PD peripheral in STM32s? If so, how?
Regards,
Caner,
Alp Lab
2025-09-30 3:23 AM - edited 2025-09-30 10:29 AM
Hi @caneralp
I'm not expert in power management, I suggest you checking the implementation provided in the demo on G0. eval STM32CubeG0 demonstration firmware - User manual section 4.3.7 Display Port demonstration.
This section 9.11. How DP does it work on EVAL-G081 demonstration.
Source code of this demo. USB PD library supports VDM (Vendor define message)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.