2016-07-25 12:02 AM
Hi
i have configured the mass storage using cubemx,but my code is not working it shows ''format disk to use'' in my system. here i have attached the configuration file can you any help me please.regardsRajesh #sd-as-usb-mass-storage2016-07-26 10:25 AM
Hi d.rajesh.001,
Try to create on only thread for the same subject. Check the following response that I gave in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F746G-%20usb%20device%20mass%20storage%20with%20RTOS¤tviews=62]thread: '' I have est the .ioc file that you shared , compile and generate code and everything is ok (no message as you indicated. Check if you are using CubeMx 4.16.0 and Firmware package STM32Cube FW_F7 V1.4.1 version. '' -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.