2018-05-08 4:11 AM
i using STMF779I-EVAL board and try to implement USB Mass Storage + SD Card . But the read/write speed i am getting when write/read from Window PC is too slow.
Read : 1MB/s; Write : 200KB/s
Even I already used DMA mechanism to speed up the SDMMC driver .
This is my implementation for read/write
int8_t STORAGE_Write_HS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{ //printf('STORAGE_Write_HS \n'); HAL_SD_CardStateTypeDef sd_card_state_return; HAL_SD_StateTypeDef state_return; uint32_t timeout = 0; if(HAL_OK != HAL_SD_WriteBlocks_DMA(&hsd1, buf, blk_addr, (uint32_t) blk_len)) { printf('Error : STORAGE_Write_HS failed Err: %u, blk_addr : %u ; blk_len : %u\n', hsd1.ErrorCode, blk_addr, blk_len); return USBD_FAIL; }// Callback
HAL_SD_TxCpltCallback increare writestatus to check writing status
while (writestatus == 0)
{}
writestatus = 0;/* Wait until SD card is ready to use for new operation */
while (HAL_SD_GetCardState(&hsd1) != HAL_SD_CARD_TRANSFER) { } return (USBD_OK); /* USER CODE END 14 */}void HAL_SD_TxCpltCallback(SD_HandleTypeDef *hsd)
{ //printf('HAL_SD_TxCpltCallback \n'); if(hsd->Instance == SDMMC1) { writestatus = 1; }}
I think that the HAL_SD_GetCardState(0 to long time to change state to HAL_SD_CARD_TRANSFER.
Could you let me know what is the root cause and is there any way to improve the speed ?
Thank you very much.
2018-05-23 12:56 AM
Hi
Turvey.Clive.002
,So how can i help you , im willing to
2018-05-23 12:34 PM
My grass always need mowing, and I have a large fence that needs reseating and repainting.
The biography on my profile page also provides some details.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.