2008-02-21 8:07 PM
USB Hard Fault Exception
2011-05-17 3:24 AM
I am using the USB Joystick HID example compiled
in GCC, running on the Keil MCBSTM32. D+ is pulled high constantly (i.e. no software disconnect). When I rebuild with a new PID and plug in, Windows XP finds the device and registers as a HID, but the processor interrupts with a Hard Fault Exception. I then have to unplug, and plug back in, after which it functions normally with no problems. Do you know what may be causing the Hard Fault Exception or how I can trace the source? This happens consistently every first plug-in.2011-05-17 3:24 AM
I have traced the cause of the exception to a read of non-existant memory in usb_core.c
Please let me know if anyone has an idea why the address returned by CopyData is wrong. usb_core.c: void DataStageIn(void) { ..... DataBuffer = (*pEPinfo->CopyData)(Length); <- Bad Address UserToPMABufferCopy(DataBuffer, GetEPTxAddr(ENDP0), Length); .....2011-05-17 3:24 AM
Dear paul,
Could you please share me your modifications vs the USB Kit on ST web site ? , I will try to do the same and investigate on the issue. is it running on a specific board ? Thx. STOne-322011-05-17 3:24 AM
Why has nobody else noticed this problem?
Windows requests a string descriptor with index 0xEE. This is out-of-bounds for the string descriptor array in the example. Surely this problem should occur for everyone (first time the device is connected) ? See: Why does Windows XP issue a string descriptor request to index 0xEE?http://www.microsoft.com/whdc/system/bus/USB/USBFAQ_intermed.mspx
2011-05-17 3:24 AM
Dear paul,
Thx for the useful details and this Mirosoft FAQ. As you said this should happen for evryone once on a new windows OS since in our USB Kit we do not respond with a stall for this strange get descriptor Request with 0xEE index , so Windows XP will issue a single-ended zero reset to the device to recover the device from an unknown state. However I assure you that the USB Kit has been sucessufully certified with the current firmware on USB.org organization. I will escalate this issue to our techs for improvement. Thx , Cheers, STOne-32.2011-05-17 3:24 AM
Hi STOne,
I am using the Keil MCBSTM32, and am not using any port (i.e. pd9/pd2) to software disconnect the usb. I have tried compiling with the exact same code as the usb example from the website (except different startup.c - i'm using anglia idealist), yet the same thing happens. I have traced it to a bad value of pInformation->USBwValue0 (0xEE), which causes a read of a non-existant array value, which creates the hard exception fault. I'll let you know if I figure out why. The offending function (and hack-around) are from usb_prop.c: u8 *Joystick_GetStringDescriptor(u16 Length) { u8 wValue0 = pInformation->USBwValue0; // can be bad value (0xEE) if (wValue0 > 3) wValue0 = 3; // hack-around return Standard_GetDescriptorData(Length, &String_Descriptor[wValue0]); }2011-05-17 3:24 AM
hi paul,
let me see if I get this straight, when an unexpected descriptor is read the core faults cause usb kit doesn't range-check the (untrusted) argument?2011-05-17 3:24 AM
Naturally, the windows issued 'single-ended zero reset' will not take the device out of the Hard Fault Exception interrupt handler (while(1);)!
This seems to be a Microsoft only thing, so it probably isn't part of the USB.org conformity test.2011-05-17 3:24 AM
Lanchon:
Correct, see Joystick_GetStringDescriptor above. This will happen the first time a device is plugged into a windows XP computer (and potentialy on other occasions/systems). Apparently the correct behaviour is to stall, although I've read (http://www.sourcequest.com/modsContent.htm) that you can get away with returning a 'minimal descriptor'. [ This message was edited by: paul.smitton on 25-02-2008 10:05 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.