2011-08-17 1:39 AM
Hello,
I saw that in usart.c there is the function USART_SendData(USART2, 'a'); but this is for only one character (here 'a'). I want to send more than one character but I can't find how. I think that USART_SendData(USART2, 'hello'); won't work. Coud anyone help me please? Thanks2014-03-25 3:24 AM
2014-03-25 3:38 AM
No, no, no. x is passed by value (not by reference) and so is local and therefore will not change the origional x.
2014-09-29 8:20 AM
Hello ther
SendData (USART, �? AT�?); and i receive OK on my hyperterminal, but when i send 2 commands i only receive 1 OK instead of 2, eventhough my delay is long.
do you know why?secondly, why do i have to to press the reset button to print the sent data on the hyperterminal? is it not better if it prints automatically?
and lastly, how do i enable the ouput pins of my stm32F4 with Sms?
thank you. Im looking forward to read you
Sorry i didnt managed to create a new thread2014-09-29 9:19 AM
Perhaps because the modem expects a CR,LF pair (Carriage Return, Line Feed)?
Yeah, I have no real idea what you're doing or how. I guess you'd talk to the modem using it's documented command set, extract and parse the SMS message data, and act upon it using functionality you program? This would require a reasonable mastery of C programming.2014-09-29 2:26 PM
in stm32f4xx.h set correcr hse value, same apply for system_config.c
If in stm32f4xx.h hse is incorrect, you will get bad boud rateWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.