2017-03-06 5:21 AM
Hi All,
I am working on STM32f103 CB and i am trying to read the RFID tag EM18 using USART1.Whenever the card is waved on the Reader, i will receive a interrupt on USART receive pin PA10. Can anybody tell how to copy the received tag in the uart interrupt handler. I am able to copy only the first byte. i want to copy the entire 12 byte in the UART receive interrupt handler .
Below is my code snippet to read the RFID TAG
void USART1_IRQHandler(void)
{ u8 i; char *t; RxBuffer[12] ='/0'; { if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) /* Read one byte from the receive data register */ for(i=0;i<12;i++){
*t = (USART_ReceiveData(USART1) & 0xFF); RxBuffer[i] =*t++; } // USART1_TX_Byte(RxBuffer[WriteDataCounter]); //Uart3Timeout = 10000; } USART_ClearITPendingBit(USART1, USART_IT_RXNE); }Can anybody tell how to implement this
Kind Regards
Don
#usart-string-receive-interrupt #stm32f103cb-usart2017-03-06 6:15 AM
The bytes arrive one at a time, copy each into a buffer, and advance the pointer. Don't sit in the IRQ Handler blocking execution.
2017-03-06 6:21 AM
Rename ' i ' into RX_Index; and make it a global variable (declared before the function, and as extern in the H file)
set RX_Index = 0;
Activate the RX interrupt
Insider the interrupt, store in buffer indexed with RX_Index
Then RX_Index++
Then if RX_Index == 12 , disable the USART RX interrupts
In the main loop, wait for RX_Index ==12 to read the buffer.
Rinse and repeat for the next batch.
2017-05-26 9:20 AM
Hey guys,
I figured I'd jump in here as I have a related problem. I'm using USART3 on an STM32F1 with a serial terminal (RealTerm) and for some reason when I send data from the terminal my USART3_IRQHandler does not fire. I've got the TX side working fine (i.e. I can send data from USART3 to my serial terminal). I've checked my code several times and can't see anything wrong with it:
void USART3_Config(void)
{ GPIO_InitTypeDef GPIO_InitStruct; NVIC_InitTypeDef NVIC_InitStructure; USART_InitTypeDef USART_InitStruct; // 1) Clock Config RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3,ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB,ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);// 2) GPIO Config
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_10; // USART3 TX GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_11; // USART3 RX GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIO_InitStruct);// 3) NVIC Config
NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority=0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // 4) USART Struct Config USART_InitStruct.USART_BaudRate = 9600; USART_InitStruct.USART_StopBits = USART_StopBits_1; USART_InitStruct.USART_WordLength = USART_WordLength_8b; USART_InitStruct.USART_Parity = USART_Parity_No; USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStruct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART3, &USART_InitStruct); // Enable RX interrupt USART_ITConfig(USART3, USART_IT_RXNE, ENABLE); USART_Cmd(USART3, ENABLE); }...
void USART3_IRQHandler(void)
{ if(USART_GetITStatus(USART3, USART_IT_RXNE) != RESET){ // Read one byte from data register RxBuffer[RxCounter++] = USART_ReceiveData(USART3); if(RxCounter == 15){ // Disable interrupt USART_ITConfig(USART3, USART_IT_RXNE, DISABLE); } }}Can anyone help me with this? Have I missed something?
Cheers,
Tony
2017-05-26 10:45 AM
Does receive work in polling mode?
Try toggling a GPIO pin.
2017-05-26 1:37 PM
Review vector table content, and linkage via .MAP file
2017-05-29 11:21 AM
Hi Clive,
I've tried polling for the data but still no joy. I also tried toggling the GPIO pin that I am using for USART3_RX (PB11) but it doesn't seem to have any effect.
I can see that USART3_IRQHandler is defined in both my vector table and my .MAP file...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.