2020-08-05 1:44 AM
Hello,
When I enable usart idle interrupt function on stm32g071rb, it fires the interrupt immediately even there is no communication on the bus.
I debug use cubeide and IAR. The results are the same.
When UE bit in USART_CR1set to 1, the IDLE bit in USART_ISR will change to 1 right now.
So after IDLE interrupt enabled, it will cause a interrupt.
I don't know why the IDLE bit in USART_ISR change to 1.
And I try to clear the IDLE bit in USART_ISR, by set IDLECF bit in USART_ICR before enable the interrupt. It no works.
But I add a delay_1_ms between uart_init and clear Idle interrupt flag, it works.
The code is below:
MX_USART1_UART_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_Delay(1); // work with this
__HAL_UART_CLEAR_IDLEFLAG(&huart1);
__HAL_UART_CLEAR_IDLEFLAG(&huart2);
__HAL_UART_ENABLE_IT(&huart1, UART_IT_IDLE);
__HAL_UART_ENABLE_IT(&huart2, UART_IT_IDLE);
2020-08-05 2:19 AM
Well, it does signal that the line has entered the IDLE condition. What is the problem here?
2020-08-05 5:14 PM
The problem is that there is no communication on the uart receive line. So it doesn't need the condition for idle interrupt.
Even I clear the interrupt flag before enable this interrupt, it seems the flag can't be cleared.
I must add a delay, later the problem disappear.
2020-08-05 8:48 PM
Possibly it doesn't trigger an idle condition until the first definitive stop bit is received, which would occur around 10 or so bits after initialization.
2020-08-05 9:39 PM
Check the sequence between gpio and usart init. if gpio is done later, for a short while the usart is exposed to the unknown floating node.... strike throught this concern by checking it.
2020-08-06 6:08 PM
Thanks for reply.
My doubt is same as you.
The init of usart is create by cubeIDE use HAL lib. I think the procedure are same between F103 and G071. Same code in F103 and G071, the phenomenon
are different. F103 is OK, but G071 is not. It confused me.
2020-08-06 6:10 PM
Thanks for reply.
The problem is that it trigger an idle condition without a communication.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.