2024-07-07 4:29 AM - last edited on 2024-07-07 5:32 AM by STOne-32
Ok, so I tried to follow
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink
for an example on how to use STM32G0B1 family as a simple USBC Power delivery sink. The Article seems to have received an update on June 2024 so it suggested to be rather up-to-date.
Unfortunately, lots (!) of things have changed when I try to reproduce the settings that are done in CubeMX in the Tutorial. For some settings I am quite sure that I found the "correspondence" in the current version of CubeIDE/CubeMX but with others, one is really lost because settings or variables just don´t exist anymore or new ones were added. It makes not even sense to ask for all of these here, because really a lot of different things in different tabs or sections have changed.
If the Wiki should allow a more or less useful "getting started" approach, this is really broken. Has anybody followed the guide with a more of less recent version of the G0 FW Libs and a more or less recent CubeIDE version? I am currently using the latest 1.16 of CubeIDE.
P.S.: Tutorials like this one is even "evil" in my opinion. It tricks the customer to think that there is at least a guide for some common use cases/scenarios which work out of the box and which the customer can base further investigation on. If there is not even a functional demo from a company like ST, then please remove the page that claims to have one.
Solved! Go to Solution.
2024-07-17 2:48 AM
@LLECH.1 : Ok. First, sorry for the rant, but to me - breaking changes happen way too often in CubeMX/CubeIDE.
BUT - I did really a lot of different tests with most recent CubeIDE 1.16 and while doing so I deleted all the Cube Versions I had ever on the PC, more or less a complete cleanup. Reinstalling everything from ground up and going through the tutorial in fact gives code that actually compiles with no errors. I would apologize since it now seems working but I really have no ideas which problem was solved by the complete wipe and reinstall since I did nothing different than before while following the video.
Anyway: Thanks for your reply on the issue! A question remains: Is there a PD Sink example/demo that comes without the need of an OS?
Thanks!
2024-07-08 12:33 AM
Hello Franz,
Thank you for your feedback, could explain a little bit more what settings or parameters you are talking about so that we can improve wiki page ? Did you try to follow this video : How to build an USBPD Sink application using the X-Cube-TCPP software pack ?
It might help you to build your own application since it is a full demonstration of where to click to build a sink application in STM32CubeMX.
Best Regards,
2024-07-17 2:48 AM
@LLECH.1 : Ok. First, sorry for the rant, but to me - breaking changes happen way too often in CubeMX/CubeIDE.
BUT - I did really a lot of different tests with most recent CubeIDE 1.16 and while doing so I deleted all the Cube Versions I had ever on the PC, more or less a complete cleanup. Reinstalling everything from ground up and going through the tutorial in fact gives code that actually compiles with no errors. I would apologize since it now seems working but I really have no ideas which problem was solved by the complete wipe and reinstall since I did nothing different than before while following the video.
Anyway: Thanks for your reply on the issue! A question remains: Is there a PD Sink example/demo that comes without the need of an OS?
Thanks!
2024-07-28 10:33 PM
@LLECH.1 : any "news" on the question about a "non-OS based" demo?
2024-08-06 8:35 AM
Hello Franz,
There is no "non-OS based" Sink PD demos as far as I know.
Best Regards,
Lucas
2024-08-06 11:46 PM
HI @LLECH.1 : Thanks, I found some thread that outlines what would be needed to make it work without OS, but for now, this is not important and for now, I will stay on the demo variant that makes use of the RTOS to avoid other possible issues.
Regarding the video you linked: I was (finally) able to get the demo working after a small fix (see SBCPD CubeIDE code results in HardFault when GUI_INTERFACE is enabled ).
However, there is a Problem left with the CubeMonitor-USBCPD for which I created a follo-up post here (STM32G0 USBCPD: Target communication/configuration via STM32CubeMonitor-UCPD ). I would appreciate your input in case you have some ideas of what and how to further investigate that issue.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.