2008-03-08 6:55 AM
UART with 8MHz internal oscillator?
2011-05-17 3:26 AM
Hi,
I am working on new board that has restriction in dimension (something new? :o) and think about using only internal oscillator(8MHz). OK, may be 32kHz for RTC if I can make it without external RTC chip (there is one ST software example about this, still need to read and test it). My question is - is it possible to make USART working (max. baud rate 57600) with internal oscillator? By STM32F103 datasheet max. oscillator error is +-3% (for -40,+105C), which is close to max. baud rate error allowed for UART. As I expect that device will be all the time in range -20, +80C oscillator error is probably lower. Also, anyone worked with CAN - what is tolerance there? This is not so critical as I am considering SPI as alternative, distance is quite short - max 20 cm. Thanks.2011-05-17 3:26 AM
my opinion is I wouldn't make a commercial device using the STM32 internal osc to drive a UART without some type of calibration scheme, just my opinion!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.