2014-07-31 12:04 PM
Hi,
There is a bug in STMCube when using UART/USART. When I config STM32F407VG and config UART4 and USART2 with MDK, then only stm32fxx_hal_uart is included. The stm32fxx_hal_uSart is not included and so is the config not useable. I have to add the stm32fxx_hal_usart.c manually to be able to use its functions.See attached file which produces only UART file and not USART files.2014-09-10 6:27 AM
Hello,
In the HAL drivers named stm32f4xx_hal_usart.c and stm32f4xx_hal_uart.c, USART and UART refer to the peripheral modes, respectively synchronous and asynchronous, and not to actual peripheral names. So, when you are configuration the USART peripheral to be in asynchronous mode, you will be using the stm32f4xx_hal_uart.c library. Another example, you may configure the USART peripheral in IrDA mode, you will find in the generated project the corresponding stm32f4xx_hal_irda.c driver. Best Regards2014-09-10 7:32 AM
''USART and UART refer to the peripheral modes, respectively synchronous and asynchronous''
So shouldn't they be ''USRT'' and ''UART'', then?!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.