2017-09-25 1:31 AM
Hello! Have some problem with UART on STM Nucleo L476RG. We need to transmit bytes from Nucleo to Raspberry (needed to output in program on Raspberry count-speed; it depends on frequency on Nucleo, that we want to transmit from Nucleo to Raspberry).
But it doesn't work (though we can transmit (write() raspberry function) bytes from Raspberry to Nucleo; and we have similar sample of read() function).
So can you help with this problem?
#uart #usartSolved! Go to Solution.
2017-09-26 8:12 AM
Hello,
Have a look to the UART example available in the STM32CubeL4 firmware package to help you on UART use and initialization.
Kind Regards
Imen
2017-09-26 8:12 AM
Hello,
Have a look to the UART example available in the STM32CubeL4 firmware package to help you on UART use and initialization.
Kind Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.