2022-03-25 1:18 PM
Hi there!
I start to use a UART (RS485) with stm32g031f6 , and i use
HAL_UART_Transmit_IT
HAL_UART_Receive_IT
and both works. So now i want implemet an timeout on RX line. I saw the app note 3109 and i have a couple of question:
My goal is use the second one the problem is i have an interrupt when i tx data and when i rx a data.
I read the data sheet and i know there is a ISR register and the bit RXNE:is set when the data is ready is coorect check if is set to one ? and is coorect do in this way USART2-> ISR & 0x20 ? and do in the interrupt UART ? or i need the check in the while loop ? and afther i receive a time out how i can reset the pointer use from the software for save the data in the array ?
Forgive me for this long question but i'm really soo confuse.
Thanks a lot
Sergio
2022-03-25 11:21 PM
Hi Sergio,
yes, checking USART2-> ISR & 0x20 in the interrupt handler is correct.
But, the app note dates back to a time when neither HAL nor G0 series existed.
If you're already using HAL, you can simply use the provides callback funtions instead of tampering with the raw UART interrupt. I.e you simply implement two functions
void HAL_UARTEx_RxFifoFullCallback(UART_HandleTypeDef *huart);
void HAL_UARTEx_TxFifoEmptyCallback(UART_HandleTypeDef *huart);and HAL will crack the register bits for you. Look also at the
HAL_UARTEx_ReceiveToIdle_DMAHAL function which might be helpful for you.
HAL is not everybody's darling and has its limitations or even shows bugs in complex scenarios. There is a detailed explanation and sample "HAL free" code in https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx .
hth
KnarfB
2022-03-26 4:41 AM
Thanks for your fast replay.
I want create a timeout because i have one master and 18 slave and if i don't receive all data i need the call again the slave from master and after a while write message on display. I think the callback function can help me to do that. I know the HAL function are no the best one and one day or another i need the start to write my own library. The last question some one have idea how clear the pointer or mabye i can just setup the rx to receive one data and create my own circula buffer.
Thanks again
Sergio
2022-03-26 6:00 AM
I think the callback function can help me to do that. Sorry i want wrote I think the callback function can't help me to do that
2022-03-26 7:44 PM
If the timeout can be in msec, clear a ram variable within the interrupt, and increase it say in systick interrupt. Once this coumter reaches a defined threshold, do something.
Of course you can make countdowns too. Interrupt priority well tuned.
2022-03-26 7:55 PM
> I want create a timeout because i have one master and 18 slave and if i don't receive all data i need the call again the slave
Then it is very simple. Just call HAL_UART_Transmit to send, then immediately HAL_UART_Receive() to get the reply. The last arg of HAL_UART_Receive is the timeout that you need. No any circular buffers.
Later replace the HAL with something better, as you already plan.
2022-03-27 2:46 AM
Thanks a lot
Sergio
2022-03-27 9:06 AM
And no any callback functions. Just keep it simple.
2022-03-27 11:34 AM
Yes is true , i just want say can't help me with timeout , because if i don't receive all data i don't receive the interrupt
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.