2018-03-11 6:33 AM
hello
i use stm32f107 and use to standard standard peripheral library but now i have use hal drive and i new on it.
i want to build a transmitter receiver.i want when receive data in mcu i get an interrupt .when i use
standard peripheral library i don't have problem and i get interrupt every a byte . i use this code but i get interrupt only one time
how can i fix that?
GPIO_InitTypeDef GPIO_InitStruct;
/* USER CODE END USART2_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_USART2_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE();/**USART2 GPIO Configuration
PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_2; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* USART2 interrupt Init */
HAL_NVIC_SetPriority(USART2_IRQn, 1, 0); HAL_NVIC_EnableIRQ(USART2_IRQn); huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }if(HAL_UART_Receive_IT(&huart2, RxBuffer1 , 2) != HAL_OK){ Error_Handler(); }void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{///////Receive Data Here }void USART2_IRQHandler()
{ HAL_UART_IRQHandler(&huart2);}
2018-03-11 1:17 PM
You have to re-enable the interrupt., it becomes cumbersome/slow and not efficient.
I don't do it that way, I use a circular DMA buffer for receive.
You can monitor the DMA pointer to see if a byte has arrived.
I check every mS,
Did you use the Cube ?
2018-03-11 11:53 PM
i can't use dma because i use for another purpose .
yes i use cube example
2018-03-11 11:55 PM
the only DMA has 12 channels;
from the datasheet;
• DMA: 12-channel DMA controller
– Supported peripherals: timers, ADCs, DAC,I2Ss, SPIs, I2Cs and USARTs2018-03-12 12:39 AM
can you give me an example with DMA circular ?
2018-03-12 12:49 AM
you have to configure it in the cube
this is not trivial for novice,
I cant do all the work for you, but here are some pointers from the '091 and '767 processes..
in the cube eonfiguration tab, Enable Rx DMA for circular buffer, enable DMA interrupt and Usart interrupt.
(I use TxDMA as a normal buffer.)
void initUart3RxDMABuffer(void) {
if (HAL_UART_Receive_DMA(&huart4, (uint8_t *)Usart3RxDMABuffer, U3RxBufSize) != HAL_OK) { // Transfer error in reception process //_Error_Handler(__FILE__, __LINE__); printf(string, 'initUart3RxDMABuffer Failed\n'); } else printf(string, 'initUart3RxDMABuffer OK!\n');}char readU3(void) {
char readByte = Usart3RxDMABuffer[U3RxBufferPtrOUT++]; if (U3RxBufferPtrOUT >= U3RxBufSize) U3RxBufferPtrOUT = 0; return readByte;}char readableU3(void) { U3RxBufferPtrIN = U3RxBufSize - huart4.hdmarx->Instance->CNDTR; return U3RxBufferPtrIN - U3RxBufferPtrOUT;}I poll the RxDMA buffer size in my foreground loop, every mS
if(readableU3()) // have at least one byte available in RxDMA buffer.
2018-03-12 1:03 AM
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.