2019-08-07 6:45 AM
I'm trying to take input from user via serial port. I use STM32's USART1_IRQHandler and sscanf functions. Although I can print message on the port by using sprintf, I can't take input with sscanf. It doesn't wait for input and assigns a value I can't understand. I shared the code below. How may I solve this issue?
char uartTxBuffer3[50];
memset(uartTxBuffer3, 0, 50);
sprintf(uartTxBuffer3, "\nEnter frequency: \n");
BSP_Uart_Transmit(uartTxBuffer3, sizeof(uartTxBuffer3));
char buffer [50];
char freqaddress[50];
int inputfreq;
USART1_IRQHandler();
//USART_ClearITPendingBit(USART1, USART_IT_RXNE);
sscanf(buffer,"%s %i",freqaddress,&inputfreq);
char uartTxBuffer4[100];
memset(uartTxBuffer4, 0, 100);
sprintf (uartTxBuffer4, "Frequency: %i",(int)inputfreq);
2019-08-07 8:37 AM
You generally don't call USART1_IRQHandler() in-line from your code. That's not how interrupts work. The micro-controller calls the handler when the interrupting device signals.
You'd need the handler to accumulate data, that arrives a byte at a time.
You'd need to wait for it to actually fill a string buffer against which to run sscanf(), the data would need to be NUL terminated.
2019-08-08 5:03 AM
Thank you for your answer. I wonder how can I call the handler in the main function? My handler function is attached below, written by another engineer and I need to set it right to establish the communication.
void USART1_IRQHandler(void) //usart irq
{
char chr;
if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET)
{
uartRxBuffer[uartIndex] = USART_ReceiveData(USART1);
uartIndex++;
if(uartIndex == 342)
{
uartIndex = 0;
uartReceiveCallBack(uartRxBuffer);
}
}
if(USART_GetITStatus(USART3, USART_IT_TXE) != RESET)
{
}
}
I can't figure out how to use this function in the main to use scanf. Please help.
2019-08-08 7:28 AM
You'd probably want to have the interrupt code check for patterns and resync, at some point a 342 byte byte might get misaligned.
The current routine calls a callback function with the data.
You'd need to copy the data to a buffer that isn't transient, and also make sure it is NUL terminated.
You could then flag the availability of data via a volatile variable, which the main() loop could wait on.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.