2017-05-29 6:26 AM
Hi,
In my project i want to use two uart in the same card (stm32F4xx), the first UART (UART6) is connected with PC and the seconde one (UART3) is connected with others cards.
It's possible to send via UART3 what i receive with UART6??
#uart #stm322017-05-29 7:38 AM
>>It's possible to send via UART3 what i receive with UART6??
Yes, you'd need to take the data received by one and send it out the other, if the baud rates are the same you might get away with just doing this in a loop, or via the IRQHandler. A more robust method would be to buffer the data to provide some elasticity.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.