2019-04-10 6:16 AM
Hi,
I am running a STML433 with external xtal. I have a serial port that works fine when I set the parity to NONE (I set the port to 9600 baud No parity 8bits 1stop bit). And works well , as expected. I have to set it to parity even (set to 9600 baud Even parity 8n bits 1 stop bit), so I set the register as follows:
USARTx->CR1 |= USART_CR1_PCE;// set parity
USARTx->CR1 &= ~USART_CR1_PS;// even parity
everything else in the uart is the same. But I dont get the correct info coming out of the serial port, the only way is if I set the terminal window on the receiving side to E 7 bits and 2 stop bits , which isnt any use. My complete setup is:
USARTx->CR1 &= ~USART_CR1_UE; //disable uart
USARTx->CR1 &= ~USART_CR1_M;// 8 bits
USARTx->CR2 &= ~USART_CR2_STOP;// 1 stop bit
if(Parity==NO_PARITY)
USARTx->CR1 &= ~USART_CR1_PCE;// no parity
else
{
//even only other option at the moment
USARTx->CR1 |= USART_CR1_PCE;// set parity
USARTx->CR1 &= ~USART_CR1_PS;// even parity
}
USARTx->CR1 &= ~USART_CR1_OVER8; //oversample
USARTx->BRR = 1666;
Anyone let me know what I am doing wrong? I am running the clock at 16MHz.
Many thanks
Scott
Solved! Go to Solution.
2019-04-10 6:37 AM
Try the cubemx initialization.
USARTx->CR1 &= ~USART_CR1_M;// 8 bits
with parity set to 9 bits
2019-04-10 6:37 AM
Try the cubemx initialization.
USARTx->CR1 &= ~USART_CR1_M;// 8 bits
with parity set to 9 bits
2019-04-10 7:02 AM
Do you have a logic analyzer (or oscilloscope) that can capture the raw data coming out of the serial port?
Have you measured the bit length, number of bits, etc?
Do you have matching settings on the receive side (9600, 8 bit, Even Parity, 1 stop bit)?
What kind of error you get when if fails? (Failed parity, overrun)?
2019-04-10 8:42 AM
Hi
This worked. I never realised I had to set to 9 bits if I wanted parity.
Many Thanks
Scott
2019-04-10 8:52 AM
Well the bit count includes parity in ST's U(S)ART implementation 7E1 would be 8-bit 8On1 would be 9-bit, for example. They also use 9-bit for "multi-processor communication" mode or whatever hack the 8051 used.
When reading the DR directly, mask the bits you want to see/remove
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.