2020-03-04 5:04 AM
Hello, second day try to launch UART in LIN mode.
Task: waiting break, when break flag set up, switch on DMA receiver.
Transmitter works fine and send 100us break before frame.
But receiver can't set UP Break Flag.
And there are not everywhere examples =(
UART initialization:
void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_LIN_Init(&huart2, UART_LINBREAKDETECTLENGTH_10B) != HAL_OK)
{
Error_Handler();
}
__HAL_UART_ENABLE_IT(&huart2, UART_IT_LBD);
HAL_UART_Receive_DMA(&huart2,(uint8_t*)UART2_RxBuffer,UART2_RX_BUFFER_SIZE);
}DMA + GPIO initialization:
__HAL_RCC_USART2_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**USART2 GPIO Configuration
PA2 ------> USART2_TX
PA3 ------> USART2_RX
*/
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USART2_RX Init */
hdma_usart2_rx.Instance = DMA1_Channel6;
hdma_usart2_rx.Init.Request = DMA_REQUEST_2;
hdma_usart2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_usart2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_usart2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_usart2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_usart2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_usart2_rx.Init.Mode = DMA_NORMAL;
hdma_usart2_rx.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_usart2_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(uartHandle,hdmarx,hdma_usart2_rx);
/* USART2 interrupt Init */
HAL_NVIC_SetPriority(USART2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART2_IRQn);Interrupt and launch DMA
void USART2_IRQHandler(void)
{
/* USER CODE BEGIN USART2_IRQn 0 */
if(__HAL_UART_GET_FLAG(&huart2,UART_FLAG_LBDF))
{
HAL_UART_Receive_DMA(&huart2,(uint8_t*)UART2_RxBuffer,UART2_RX_BUFFER_SIZE);
__HAL_UART_CLEAR_FLAG(&huart2,UART_FLAG_LBDF);
UART2_PacketReceived=true;
}
/* USER CODE END USART2_IRQn 0 */
HAL_UART_IRQHandler(&huart2);
/* USER CODE BEGIN USART2_IRQn 1 */
/* USER CODE END USART2_IRQn 1 */
}Main:
while (1)
{
/* USER CODE END WHILE */
if(UART2_PacketReceived==true)
{
__HAL_UART_DISABLE_IT(&huart2, UART_IT_LBD);
HAL_Delay(10);
HAL_UART_DMAStop (&huart2);
UART2_PacketReceived=false;
__HAL_UART_ENABLE_IT(&huart2, UART_IT_LBD);
}
/* USER CODE BEGIN 3 */
}Currently interrupt work, DMA also work but UART receiver lost a lot of bytes or skip a lot of frames.
Please help me :sad_but_relieved_face:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.