2017-11-20 11:52 AM
MCU: STM32F777II
I have configured DMA for RX on the UART as:
/* UART7 DMA Init */
/* UART7_RX Init */ hdma_uart7_rx.Instance = DMA1_Stream3; hdma_uart7_rx.Init.Channel = DMA_CHANNEL_5; hdma_uart7_rx.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_uart7_rx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_uart7_rx.Init.MemInc = DMA_MINC_ENABLE; hdma_uart7_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_uart7_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_uart7_rx.Init.Mode = DMA_CIRCULAR; hdma_uart7_rx.Init.Priority = DMA_PRIORITY_MEDIUM; hdma_uart7_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;Just wanted to when I fire off a DMA read using the HAP api:
HAL_UART_Receive_DMA(&UART_DOWN_USB_TO_SERIAL, (uint8_t*)&holder, 1);
Do I need to call HAL_UART_Receive_DMA() again in the HAL_UART_RxCpltCallback callback function, or it was required only once provided I need to continue reading it infinitely?
#uart #dmaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.