2020-03-23 3:27 AM
Hi,
UART stops transmitting (both IT and polling modes) after entering and exiting from STOP 2 mode.
Although I'm renabling the UART when I'm exiting STOP 2 I don't see the data received on the other side.
When I'm connected to MCU via JTAG everything works well because the JTAG blocks the MCU from entering STOP 2. Once I disconnect the JTAG and reset the device, it does enter STOP 2 mode but the UART stops funciotioning.
Any thoughts?
Anything else I need to enable when I exit STOP 2?
If that matters, I use RTC as the wake up source, and the STOP 2 mode is configured with WFI.
Thanks!
2020-03-23 5:44 AM
You're likely just missing something on re-initialization after it exits stop mode. stm32l4xx_hal_pwr.c lists the requirements after exiting stop mode.
2020-03-25 2:59 AM
Thanks.
Any idea on how to save the state of GPIO's prior to entering STOP 2 mode, and then read the IO state when exiting low power?
2020-03-25 6:31 AM
From the reference manual:
> SRAM1, SRAM2 and register contents are preserved.
So save stuff there. Or you could save to flash if you have a page available.
Also from the manual:
> In the Stop 2 mode, all I/O pins keep the same state as in the Run mode.
So no need to re-initialize GPIO pins.
2020-03-27 5:22 AM
2020-04-02 9:55 AM
Do you think that STOP2 can work as the sleep mode when using FreeRTOS' tickless idle feature?
obviously one would have to rewrite the preSleepProcess and postSleepProcess functions, but theoretically would going in and out of STOP2 using so rapidly using the IDLE task would still hold the OS's scheduler performance and everything else?
Do you know of an example for that?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.