2009-07-29 9:12 PM
UART 4 Problem
2011-05-17 4:19 AM
Im using UART4 on the STM32F103Ze.
As soon as an UART4 RX Interrupt occurs, a hard fault exception occurs Hard fault Status Register = 0x40000000 (bit 30 is set) As far as I know this indicates one of the following faults: 1. Bus fault, 2. Memory management fault 3. Usage fault Below is my code. UART initialization RCC->APB1ENR |= RCC_APB1Periph_UART4; //Enable clock for USART4 UART4->BRR = 0x0EA6; //Set baudrate UART4->CR1 = 0x00000000; //Set Data, Stop bits & Flow control UART4->CR1 |= (USART_CR1_RE | USART_CR1_TE); //RX, TX enable UART4->CR1 |= 0x20; //RXNE Interrupt Enable UART4->CR1 |= USART_CR1_UE; //USART enable Interrupt initialization NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); Interrupt void UART4_IRQHandler(void) { u8 Rx_Char; if(UART4->SR & USART_FLAG_RXNE) //RX Character { UART4->SR &= ~USART_FLAG_RXNE; //Clear interrupt flag Rx_Char = UART4->DR & 0xFF; UART4_Flag = 0xFF; } } I used the same code for USART1, 2 and 3, all working.2011-05-17 4:19 AM
Are you sure UART4 is on APB1?
2011-05-17 4:19 AM
Hi St7
According to the User Manual on p36, UART4 is on APB1. Is there something else that I am missing? Thanx2011-05-17 4:19 AM
Make sure that the address of UART4_IRQHandler is installed at the correct location in the vector table.
2011-05-17 4:19 AM
You could install a hard fault handler, maybe it'll provide some hint.
ie. something like (made for GCC): void __attribute__ ((naked)) HardFaultException() { asm volatile ( ''mov r1, #1\n\t'' ''b generic_exception_handler\n\t'' ); } /* TST LR, #4 ITE EQ MRSEQ R0, MSP MRSNE R0, PSP B hard_fault_handler_c */ void __attribute__ ((naked)) generic_exception_handler() { asm volatile ( ''tst lr, #4\n\t'' ''ite eq\n\t'' ''mrseq r0, msp\n\t'' ''mrsne r0, psp\n\t'' ''stmfd sp!, {r4-r11}\n\t'' ''mov r2, sp\n\t'' ''b generic_exception_handler_c\n\t'' ); } /* my precious debugging function * HardFault is triggered on ie. invalid memory access. * note: on IMPRECISERR, this doesn't help much. it just means that some * invalid access occured but possibly before (after/prediction?) PC */ void generic_exception_handler_c(unsigned int *oldstack, int exception, unsigned int *newstack) { int oldstack_valid = (oldstack >= (unsigned int*)&_sdata && oldstack < newstack); volatile int ffs = 1; usart_setflag(USART_DEBUG, FLAG_DIRECT, 1); if (usart_getflag(USART_DEBUG, FLAG_ACTIVE)) while (1); printf(''%s was caled, dumping regs:\n'', exception_strings[exception]); if (oldstack_valid) { printf(''r0\t0x%08x\t%i\n'', oldstack[0], oldstack[0]); printf(''r1\t0x%08x\t%i\n'', oldstack[1], oldstack[1]); printf(''r2\t0x%08x\t%i\n'', oldstack[2], oldstack[2]); printf(''r3\t0x%08x\t%i\n'', oldstack[3], oldstack[3]); } else { printf(''sp\t0x%08x\t%i\n'', (unsigned int)oldstack, (unsigned int)oldstack); printf(''sp is invalid, so some registers are missing\n''); } printf(''r4\t0x%08x\t%i\n'', newstack[0], newstack[0]); printf(''r5\t0x%08x\t%i\n'', newstack[1], newstack[1]); printf(''r6\t0x%08x\t%i\n'', newstack[2], newstack[2]); printf(''r7\t0x%08x\t%i\n'', newstack[3], newstack[3]); printf(''r8\t0x%08x\t%i\n'', newstack[4], newstack[4]); printf(''r9\t0x%08x\t%i\n'', newstack[5], newstack[5]); printf(''r10/sl\t0x%08x\t%i\n'', newstack[6], newstack[6]); printf(''r11/fp\t0x%08x\t%i\n'', newstack[7], newstack[7]); if (oldstack_valid) { printf(''r12/ip\t0x%08x\t%i\n'', oldstack[4], oldstack[4]); printf(''sp\t0x%08x\t%i\n'', (unsigned int)oldstack, (unsigned int)oldstack); printf(''lr\t0x%08x\t%i\n'', oldstack[5], oldstack[5]); printf(''pc\t0x%08x\t%i\n'', oldstack[6], oldstack[6]); printf(''psr\t0x%08x\t%i\n'', oldstack[7], oldstack[7]); } printf(''CFSR\t0x%08x\n'', *(unsigned int*)0xe000ed28); printf(''HFSR\t0x%08x\n'', *(unsigned int*)0xe000ed2c); printf(''DFSR\t0x%08x\n'', *(unsigned int*)0xe000ed30); printf(''MMAR\t0x%08x\n'', *(unsigned int*)0xe000ed34); printf(''BFAR\t0x%08x\n'', *(unsigned int*)0xe000ed38); printf(''AFSR\t0x%08x\n'', *(unsigned int*)0xe000ed3c); printf(''\nhalted\n''); while (ffs) ; } Ah, fuck, code tag doesn't work for this... code :p2011-05-17 4:19 AM
Quote:
Ah, fuck, code tag doesn't work for this... code :p
I know - it's pretty useless having a 'CODE' tag that doesn't actually work with source code, isn't it?! Who chose this forum software with such an obvious and fundamental flaw?! Previously noted nearly a year ago: [ This message was edited by: st7 on 30-07-2009 09:47 ] See also: [ This message was edited by: st7 on 30-07-2009 09:48 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.