2016-05-20 1:19 AM
Hi folks,
I have installed MX plugin 4.14.0.201603171736 into an existing eclipse Mars.2 (4.5.2). Looks like it worked. But when I try to show an STM32CubeMX window, it simply crashes my eclipse. I was expecting being able to edit a customer supplied .ioc file. Is this possible ? Is this plugin known to work with Mars.2 ? Thanks for clarifications.2016-05-20 5:06 AM
For those interrested in, a short log is pasted hereafter.
On my side I downloaded the standalone application which just work fine.#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0xed9d335f, pid=7025, tid=4149466880
#
# JRE version: OpenJDK Runtime Environment (7.0_91-b02) (build 1.7.0_91-b02)
# Java VM: OpenJDK Client VM (91-b01 mixed mode, sharing linux-x86 )
# Derivative: IcedTea 2.6.3
# Distribution: Debian GNU/Linux 8.2 (jessie), package 7u91-2.6.3-1~deb8u1
# Problematic frame:
# C [libgdk-x11-2.0.so.0+0x4735f] gdk_display_open+0x4f
#
# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try ''ulimit -c unlimited'' before
#
# If you would like to submit a bug report, please include
# instructions on how to reproduce the bug and visit:
# http://icedtea.classpath.org/bugzilla
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.