2017-11-25 11:58 AM
Hi all,
I'm working on a STM32F446E connected to a FTDI FT801 LCD. I am stacked on the commands communication on the SPI between the Micro and the LCD Controller. I have to load a couple of images on the LCD but I didn't found a proper guide on the net. There are a lot of guides for what concern the LCD controller, the ones that I have read don't explain anything about the right sequence of instructions to invoke on the micro.
Up to now I tried this:
Address_RAM_CMD = 0x908000;
SPI_Send_RAM_CMD(Address_RAM_CMD, DLSTART, 7);
SPI_Send_RAM_CMD(Address_RAM_CMD,CLEAR, 7);
SPI_Send_RAM_CMD(Address_RAM_CMD, INFLATE, 7);
SPI_Send_RAM_CMD(Address_RAM_CMD, 0, 7);
// Destination starting address in Graphics RAM
while (filesize > 0) {
f_read(&MyFile_R, data, sizeof(data), (UINT*) &bytesread);
SPI_Send_RAM_CMD(Address_RAM_CMD, data, 7);
filesize -= 4;
}
SPI_Send_RAM_CMD(Address_RAM_CMD, BITMAP_HANDLE(0),7);
SPI_Send_RAM_CMD(Address_RAM_CMD, BITMAP_SOURCE(0),7);
SPI_Send_RAM_CMD(Address_RAM_CMD, BITMAP_LAYOUT(0x00, 946, 92) ,7);
SPI_Send_RAM_CMD(Address_RAM_CMD, BITMAP_SIZE(NEAREST,BORDER,BORDER, image_width, image_height),7);
SPI_Send_RAM_CMD(Address_RAM_CMD, BEGIN(BITMAPS), 7);
SPI_Send_RAM_CMD(Address_RAM_CMD, VERTEX2II(4, 76, 27, 0), 7);
SPI_Send_RAM_CMD(Address_RAM_CMD, END, 7);
SPI_Send_RAM_CMD(Address_RAM_CMD, DISPLAY, 7);
SPI_Send_RAM_CMD(Address_RAM_CMD, SWAP, 7);
HAL_Delay(1000);
Where:
// This function is used to transmit data with SPI
// Address = address in the FTDI801 memory map
// Data = data to write in the FTDI801 memory map
// Size = number of bytes to write (Address + Data)
void
SPI_Send_RAM_CMD(uint32_t
Address,uint32_t
Data,uint16_t
Size){
uint8_t
buffer[7];buffer[0] = ((Address >> 16) & 0xFF);
buffer[1] = ((Address >> 8) & 0xFF);
buffer[2] = (Address & 0xFF);
buffer[3] = (Data & 0xFF);
buffer[4] = ((Data >> 8) & 0xFF);
buffer[5] = ((Data >> 16) & 0xFF);
buffer[6] = ((Data >> 24) & 0xFF);
HAL_GPIO_WritePin
(GPIOG, GPIO_PIN_14,GPIO_PIN_RESET
);
HAL_SPI_Transmit
(&spi_handle_structure, buffer, Size, 10000);
HAL_GPIO_WritePin
(GPIOG, GPIO_PIN_14,GPIO_PIN_SET
);Address_RAM_CMD = Address_RAM_CMD + 0x0000004;
SPI_Send(0x9024E8,(
uint16_t
)(Address_RAM_CMD-0x00908000),7);
// REG_CMD_WRITE
}
void
SPI_Send(uint32_t
Address,uint32_t
Data,uint16_t
Size){
uint8_t
buffer[7];buffer[0] = ((Address >> 16) & 0xFF);
buffer[1] = ((Address >> 8) & 0xFF);
buffer[2] = (Address & 0xFF);
buffer[3] = (Data & 0xFF);
buffer[4] = ((Data >> 8) & 0xFF);
buffer[5] = ((Data >> 16) & 0xFF);
buffer[6] = ((Data >> 24) & 0xFF);
HAL_GPIO_WritePin
(GPIOG, GPIO_PIN_14,GPIO_PIN_RESET
);
HAL_SPI_Transmit
(&spi_handle_structure, buffer, Size, 10000);
HAL_GPIO_WritePin
(GPIOG, GPIO_PIN_14,GPIO_PIN_SET
);}
With this implementation, no image is shown on the LCD.
It seems to me that the image data are not sent to the GPU RAM.
Thanks in advance.
Cheers,
Anna
2017-12-11 1:14 PM
2017-12-11 8:25 PM
Are you comfortable porting arduino code to stm32? If yes, download the sample application source from
and see how they get an 8bitter to do it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.