2008-12-16 4:27 AM
triggering adc1 from Timer 1 Capture Compare Interupt
2011-05-17 3:51 AM
I'm out of ideas. The only otehr difference I can see between yours and mine, is wherer I call ADC_DMACmd(). I don't call it until after the calibration is complete.
Try triggering a single conversion only ADC_DeInit(ADC1); lsADC_InitStruct.ADC_Mode = ADC_Mode_Independent; lsADC_InitStruct.ADC_ScanConvMode = DISABLE; lsADC_InitStruct.ADC_ContinuousConvMode = DISABLE; lsADC_InitStruct.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC3; lsADC_InitStruct.ADC_DataAlign = ADC_DataAlign_Right; lsADC_InitStruct.ADC_NbrOfChannel = 1; ADC_Init(ADC1, &lsADC_InitStruct); ADC_RegularChannelConfig(ADC1,ADC_Channel_0, 1,ADC_SampleTime_55Cycles5); etc...2011-05-17 3:51 AM
Site wont let me attach C file, but I could attach a gzip file. Go figure...
Brian F.2011-05-17 3:51 AM
Gareth,
You are correct of course. The second call to ADC_Cmd() is not necessary when you are using an external trigger (as I have discovered). Either ADON -or- external trigger is required. Brian F.2011-05-17 3:51 AM
Cheers for your help Brian.
I shall look into this further today and get back to you2011-05-17 3:51 AM
Hi all, sorry for the very late reply on this topic. I finaly found a solution/the problem a few weeks back. It seems that on the MCBSTM32E eval board not all the GPIO pins are physicaly connected to their labelled pads. This was the case with the interupt line i was attempting to use and hence the issue.
Hope that helpsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.