2022-02-11 6:33 AM
Hello,
I need to sample an ADC at 20ms using SPI. I setup a timer interrupt to do this, but I would like to fill a double buffer at SPI_RxHalfCplt and RXCplt.
My timer seems to be working correctly, however the Rx Half Complete Callback is being Called every time the timer interrupt is called.
What I really want is for the RxHalf Complete Callback to be called when half of the buffer is full.
What am I doing wrong?
#define BUFFER_SIZE 492
/* USER CODE BEGIN PV */
uint8_t Audio_Data[BUFFER_SIZE];
/* USER CODE END PV *//* USER CODE BEGIN 2 */
HAL_TIM_Base_Start_IT(&htim16); // Start Timer16
HAL_SPI_Receive_DMA(&hspi1, Audio_Data, BUFFER_SIZE);
/* USER CODE END 2 */
/* USER CODE BEGIN 4 */
void HAL_SPI_RxHalfCpltCallback(SPI_HandleTypeDef *hspi1)
{
HAL_GPIO_TogglePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin);
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi1)
{
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == htim16.Instance)
{
HAL_SPI_Receive_DMA(&hspi1, Audio_Data, 2);
}
}
/* USER CODE END 4 */
2022-02-11 10:51 AM
> HAL_SPI_Receive_DMA(&hspi1, Audio_Data, 2);
You only receive 2 bytes here. Intentional? Why would it be different than BUFFER_SIZE?
Monitor HAL return values to verify you're not trying to restart the transfer mid-transfer.
> however the Rx Half Complete Callback is being Called every time the timer interrupt is called.
You do 1 transfer per timer interrupt, so it makes sense that HT and TC interrupt would be called once per timer interrupt.
2022-02-11 11:00 AM
I only want to take one sample (16-bit) from the ADC each time the timer interrupt is triggered. However, I would like to know when the data buffer is half full and full in order to do a ping pong structure with the data. Is this possible?
2022-02-11 11:28 AM
So if I want ping pong a double buffer of size 492 bytes, but want to sample the ADC at 20ms, would I set the timer up to trigger at 20ms * BUFFER_SIZE? Which would fill the whole buffer at my sample rate and trigger the DMA receive half complete and full complete at the appropriate times?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.