2022-10-30 3:52 AM
Dear Sir.
I migrated the code of TSV_BasicAcquisition_Interrupt to my board .
The IO rae different than the example
Example Custom Board,
PC7 PB6
PC6 PB5
PB13 PB12
PB14 PB13
I keep getting HAL_TSC_ErrorCallback,
Please Advise.
Solved! Go to Solution.
2022-11-07 4:56 AM
Hello,
Do not forget to update also GPIO settings in HAL_TSC_MspInit api.
HAL_TSC_MspInit should be located in stm32u5xx_hal_msp.c (for U5 example).
Regarding HAL_TSC_ErrorCallback source
Usually this api is called by driver on error cases. See stm32u5xx_hal_tsc.c file comments:
[..]
This function allows to reset following callbacks:
(+) ConvCpltCallback : callback for conversion complete process.
(+) ErrorCallback : callback for error detection.
(+) MspInitCallback : callback for Msp Init.
(+) MspDeInitCallback : callback for Msp DeInit.
This api is called by Interrupt handler (HAL_TSC_IRQHandler) in our case.
If you need to update or rewrite HAL_TSC_ErrorCallback code, copy paste this code:
__weak void HAL_TSC_ErrorCallback(TSC_HandleTypeDef *htsc)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(htsc);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_TSC_ErrorCallback could be implemented in the user file.
*/
}
into your main.c file without "__weak" keyword:
void HAL_TSC_ErrorCallback(TSC_HandleTypeDef *htsc)
{
my own way to handle errors
}
Regarding TKEY capacitance
You mean the Sensor capacitance or the Sampling capacitance?
Usually sensor capacitances around few pF (from 2pf to 15pF I will says).
Some tools allow to compute this value according PCB and overlay materials.
(See SENSE tool from Fieldscale for example).
Usually Sampling capacitance are from 10nF to 47nF.
See AN5105 "Getting started with touch sensing control on STM32 microcontrollers" for intormation.
Regards.
2022-11-07 4:56 AM
Hello,
Do not forget to update also GPIO settings in HAL_TSC_MspInit api.
HAL_TSC_MspInit should be located in stm32u5xx_hal_msp.c (for U5 example).
Regarding HAL_TSC_ErrorCallback source
Usually this api is called by driver on error cases. See stm32u5xx_hal_tsc.c file comments:
[..]
This function allows to reset following callbacks:
(+) ConvCpltCallback : callback for conversion complete process.
(+) ErrorCallback : callback for error detection.
(+) MspInitCallback : callback for Msp Init.
(+) MspDeInitCallback : callback for Msp DeInit.
This api is called by Interrupt handler (HAL_TSC_IRQHandler) in our case.
If you need to update or rewrite HAL_TSC_ErrorCallback code, copy paste this code:
__weak void HAL_TSC_ErrorCallback(TSC_HandleTypeDef *htsc)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(htsc);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_TSC_ErrorCallback could be implemented in the user file.
*/
}
into your main.c file without "__weak" keyword:
void HAL_TSC_ErrorCallback(TSC_HandleTypeDef *htsc)
{
my own way to handle errors
}
Regarding TKEY capacitance
You mean the Sensor capacitance or the Sampling capacitance?
Usually sensor capacitances around few pF (from 2pf to 15pF I will says).
Some tools allow to compute this value according PCB and overlay materials.
(See SENSE tool from Fieldscale for example).
Usually Sampling capacitance are from 10nF to 47nF.
See AN5105 "Getting started with touch sensing control on STM32 microcontrollers" for intormation.
Regards.
2022-11-07 5:17 AM
Hi
Thanks it is working
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.