2022-12-14 12:45 AM - last edited on 2023-09-01 9:26 AM by Amel NASRI
I want to toggle a led when an external interrupt happened. But I could not.
That's my code using keil mdk for stm32f103c8t6
Any help, please?
#include "stm32f10x.h"
void GPIO_Config (void)
{
RCC->APB2ENR |= (1<<2); // Enable GPIOA clock
GPIOA->CRL &= ~(0xf<<4); // clear bits (7:6:5:4)
GPIOA->CRL |= (8<<4); // Bits (7:6:5:4) = 1:0:0:0 --> PA1 in Input Mode in Pull-up/ Pull-down mode
GPIOA->ODR |= (1<<1); // --> PA1 is in Pull UP mode
}
void EXTI1_IRQHandler(void)
{
if (EXTI->PR & (1<<1)) // If the PA1 triggered the interrupt
{
EXTI->PR |= (1<<1); // Clear the interrupt flag by writing a 1
toggle_GP(PC,13);
}
}
void Interrupt_Config (void)
{
RCC->APB2ENR |= (1<<0); // Enable AFIO CLOCK
AFIO->EXTICR[0] &= ~(0xf<<4); // Bits[7:6:5:4] = (0:0:0:0) -> configure EXTI1 line for PA1
EXTI->IMR |= (1<<1); // Bit[1] = 1 --> Disable the Mask on EXTI 1
EXTI->RTSR |= (1<<1); // Enable Rising Edge Trigger for PA1
EXTI->FTSR &= ~(1<<1); // Disable Falling Edge Trigger for PA1
NVIC_SetPriority (EXTI1_IRQn, 1); // Set Priority
NVIC_SetVector(EXTI1_IRQn, (uint32_t)&EXTI1_IRQHandler);
NVIC_EnableIRQ (EXTI1_IRQn); // Enable Interrupt
}
int main()
{
GPIO_Config();
init_GP(PC,13,OUT50,O_GP_PP); // initialize PC13 as output for toggle
toggle_GP(PC,13);
Interrupt_Config();
}
2022-12-14 12:52 AM
Yes, you can.
2022-12-14 1:04 AM
Yes, but it didn't work
2022-12-14 1:39 AM
Seems to be the old 2007 STM32F103 with blue pill and std lib?
2022-12-14 2:21 AM
Rule #1: Do not use external interrupts with buttons. (Of course, there are exceptions to this rule.)
Use timer interrupt - SysTick is a good candidate. Check the state of the button every, say, 20 ms. Record the previous state and compare it with the current state. If there is a change, react. Then record the current state as the prevoius one to be used during the next check.
If you want to use external interrupt, then you also must use time interrupt. So, the timer interrupt must be used anyway.
2022-12-14 6:41 AM
Generate your code with wizard or read reference manuals. APB2 isnt only one control required...
Try CubeMX
2022-12-14 9:14 AM
2022-12-31 3:02 AM
This video shows how to use EXTI interrupt to debounce a button and even count button presses.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.