2019-02-17 10:26 PM
We are using STM32F767BGT6 controller and S25FL128LAGMFI010 NOR Flash .
I want to do Timing analysis between this two ic's .
Below is the formula used for calculating setup margin and hold margin.
SETUP MARGIN =CLOCK PERIOD-TCO(MAX)-TSU,
HOLD MARGIN=TCO(MIN)-TH,
In this TCO is the Clock to Output Propagation delay.
Which parameter should i take in datasheet to calculate TCO?
or suggest any other timing analysis document
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.