2017-01-24 8:38 AM
Why timer IC mode doent work?
I've configured everything thround Cube, enabled interups and cant get it to work. Some channels just doent work.
__IO uint64_t impData=0;
__IO uint32_t icnt=0;...
main part
__HAL_RCC_TIM2_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_DMA1_CLK_ENABLE(); __HAL_RCC_USART1_CLK_ENABLE(); pin.Pin=GPIO_PIN_2; pin.Mode=GPIO_MODE_AF_PP; pin.Pull=GPIO_NOPULL; pin.Speed=GPIO_SPEED_FREQ_LOW; pin.Alternate=GPIO_AF1_TIM2; HAL_GPIO_Init(GPIOA,&pin); TIM_MasterConfigTypeDef smcfg; TIM_IC_InitTypeDef scfgIC; timIC.Instance=TIM2; timIC.Init.Prescaler=0; timIC.Init.CounterMode=TIM_COUNTERMODE_UP; timIC.Init.Period=0; timIC.Init.ClockDivision=TIM_CLOCKDIVISION_DIV1; if(HAL_TIM_IC_Init(&timIC)!=HAL_OK)err('v'); smcfg.MasterOutputTrigger=TIM_TRGO_RESET; smcfg.MasterSlaveMode=TIM_MASTERSLAVEMODE_DISABLE; if(HAL_TIMEx_MasterConfigSynchronization(&timIC,&smcfg)!=HAL_OK)err('z'); scfgIC.ICPolarity=TIM_INPUTCHANNELPOLARITY_RISING; scfgIC.ICSelection=TIM_ICSELECTION_DIRECTTI; scfgIC.ICPrescaler=TIM_ICPSC_DIV1; scfgIC.ICFilter=0; if(HAL_TIM_IC_ConfigChannel(&timIC,&scfgIC,TIM_CHANNEL_3)!=HAL_OK)err('x'); scfgIC.ICSelection=TIM_ICSELECTION_INDIRECTTI; if(HAL_TIM_IC_ConfigChannel(&timIC,&scfgIC,TIM_CHANNEL_4)!=HAL_OK)err('y');HAL_NVIC_SetPriority(DMA1_Channel4_IRQn,1,1); // dma uart T
HAL_NVIC_EnableIRQ(DMA1_Channel4_IRQn); HAL_NVIC_SetPriority(DMA1_Channel5_IRQn,1,1); // dma uart R HAL_NVIC_EnableIRQ(DMA1_Channel5_IRQn); HAL_NVIC_SetPriority(USART1_IRQn,2,2); // uart interupts HAL_NVIC_EnableIRQ(USART1_IRQn); HAL_UART_Receive_DMA(&uart,rbuf,4); // uart recieve HAL_NVIC_SetPriority(TIM2_IRQn,3,3); // tim IC HAL_NVIC_EnableIRQ(TIM2_IRQn); HAL_NVIC_SetPriority(TIM3_IRQn,4,4); // ticking for uart HAL_NVIC_EnableIRQ(TIM3_IRQn);and interupt itself
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef*timIC)
{if(ready!=SET)return; impData+=HAL_TIM_ReadCapturedValue(timIC,TIM_CHANNEL_3); icnt++;}uart checkes for values every 0.1 secs.
What am i doing wrong?
MCU is STM32F373CC
2017-01-24 8:59 AM
What are the symptoms and how do they fail short of expectations?
timIC.Init.Period=0;
Really?
JW
2017-01-24 9:17 AM
Hi
sher.evgeni
,timIC.Init.Period=0; //the automatic reload value ARR
The timer will count from 0 to the value stored in Auto-reload register. You should use a period value different from 0.I advise you to refer to the 'TIM_InputCapture' example provided in STM32CubeF3 package.
You find the example under the path below: STM32Cube_FW_F3_V1.7.0\Projects\STM32373C_EVAL\Examples\TIMKhouloud.
2017-01-25 4:07 AM
Thanks. That helped
2017-01-25 6:55 AM
Is it posible to combine 2 timers length for IC mode?
2017-01-25 7:39 AM
Please explain further what do you want to achieve.
JW
2017-01-25 7:48 AM
I'm trying to get timer period 32+16=48bit length
2017-01-25 9:07 AM
Hello
sher.evgeni
,There is an example titled 'TIM_CascadeSynchro' under the
package. Itshows how to synchronize TIM peripherals in cascade mode. I advise you to take it as a reference, it will be really helpful.The example isfound under the path below:
STM32Cube_FW_F4_V1.0\Projects\STM324x9I_EVAL\Examples\TIM\
TIM_CascadeSynchro
Khouloud
2017-02-20 8:24 AM
,
,
Strange situation.
Controller on stm32f373cc cant measure signal under 0.13 mSec. It just gives out constant as 0.13
STM32F407VGT disco board measured frequancy limited hundrets of nano secs.
♯ include 'main.h',
♯ include 'stm32f3xx_hal.h',
DMA_HandleTypeDef dmaUT,,
DMA_HandleTypeDef dmaA,,
UART_HandleTypeDef uart,,
TIM_HandleTypeDef tim,,
TIM_HandleTypeDef timIC,,
__IO ITStatus ready=SET,,
__IO uint64_t impData=0,,
__IO uint32_t impCnt=0,,
uint8_t tbuf[12]='000000000000',,
void err(char c){tbuf[0]=c,},
void NMI_Handler(void){},
void HardFault_Handler(void){err('1'),},
void MemManage_Handler(void){err('2'),},
void BusFault_Handler(void){err('3'),},
void UsageFault_Handler(void){err('4'),},
void SVC_Handler(void){},
void DebugMon_Handler(void){},
void PendSV_Handler(void){},
void SysTick_Handler(void),
{HAL_IncTick(),,
,HAL_SYSTICK_IRQHandler(),},
void DMA1_Channel4_IRQHandler(void){HAL_DMA_IRQHandler(&,dmaUT),},
void USART1_IRQHandler(void){HAL_UART_IRQHandler(&,uart),},
void HAL_UART_ErrorCallback(UART_HandleTypeDef*UartHandle){err('5'),},
void HAL_UART_TxCpltCallback(UART_HandleTypeDef*UartHandle){ready=SET,},
void TIM3_IRQHandler(void),
{if(__HAL_TIM_GET_FLAG(&,tim,TIM_FLAG_UPDATE)!=RESET),
,{if(__HAL_TIM_GET_ITSTATUS(&,tim,TIM_IT_UPDATE)!=RESET),
, {__HAL_TIM_CLEAR_FLAG(&,tim,TIM_FLAG_UPDATE),,
, , ready=RESET,,
, , uint8_t i,p,,
, , if(impCnt>,0),
, , {impData/=impCnt,,
, , , for(p=8,i=impData%16,impData>,0,impData/=16)tbuf[p--]=i>,9?i+87:i+48,},
, , if(HAL_UART_Transmit_DMA(&,uart,tbuf,12)!=HAL_OK)err('6'),,
, , while(ready!=SET),,
, , for(uint8_t i=1,i<,12,i++)tbuf[i]=48,,
, , impData=0,,
, , impCnt=0,}}},
void TIM2_IRQHandler(void){HAL_TIM_IRQHandler(&,timIC),},
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef*timIC),
{if(ready!=SET||impCnt>,999)return,,
,impData+=__HAL_TIM_GetCompare(timIC,TIM_CHANNEL_4),,
,impCnt++,,
,__HAL_TIM_SetCounter(timIC,0),}int main(void),
{RCC_OscInitTypeDef RCC_OscInitStruct,,
,RCC_ClkInitTypeDef RCC_ClkInitStruct,,
,GPIO_InitTypeDef pin,,
,TIM_IC_InitTypeDef scfgIC,,
,TIM_MasterConfigTypeDef smst,,
,HAL_Init(),,
,__HAL_RCC_SYSCFG_CLK_ENABLE(),,
,HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4),,
,HAL_NVIC_SetPriority(MemoryManagement_IRQn,0,0),,
,HAL_NVIC_SetPriority(BusFault_IRQn,0,0),,
,HAL_NVIC_SetPriority(UsageFault_IRQn,0,0),,
,HAL_NVIC_SetPriority(SVCall_IRQn,0,0),,
,HAL_NVIC_SetPriority(DebugMonitor_IRQn,0,0),,
,HAL_NVIC_SetPriority(PendSV_IRQn,0,0),,
,HAL_NVIC_SetPriority(SysTick_IRQn,0,0),,
,RCC_PeriphCLKInitTypeDef PeriphClkInit,,
,RCC_OscInitStruct.OscillatorType=RCC_OSCILLATORTYPE_HSE,,
,RCC_OscInitStruct.HSEState=RCC_HSE_ON,,
,RCC_OscInitStruct.HSEPredivValue=RCC_HSE_PREDIV_DIV1,,
,RCC_OscInitStruct.HSIState=RCC_HSI_ON,,
,RCC_OscInitStruct.PLL.PLLState=RCC_PLL_ON,,
,RCC_OscInitStruct.PLL.PLLSource=RCC_PLLSOURCE_HSE,,
,RCC_OscInitStruct.PLL.PLLMUL=RCC_PLL_MUL9,,
,if(HAL_RCC_OscConfig(&,RCC_OscInitStruct)!=HAL_OK)err('7'),,
,RCC_ClkInitStruct.ClockType=RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2,,
,RCC_ClkInitStruct.SYSCLKSource=RCC_SYSCLKSOURCE_PLLCLK,,
,RCC_ClkInitStruct.AHBCLKDivider=RCC_SYSCLK_DIV1,,
,RCC_ClkInitStruct.APB1CLKDivider=RCC_HCLK_DIV2,,
,RCC_ClkInitStruct.APB2CLKDivider=RCC_HCLK_DIV1,,
,if(HAL_RCC_ClockConfig(&,RCC_ClkInitStruct,FLASH_LATENCY_2)!=HAL_OK)err('8'),,
,PeriphClkInit.PeriphClockSelection=RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_ADC1,,
,PeriphClkInit.Usart1ClockSelection=RCC_USART1CLKSOURCE_PCLK2,,
,PeriphClkInit.Adc1ClockSelection=RCC_ADC1PCLK2_DIV2,,
,if(HAL_RCCEx_PeriphCLKConfig(&,PeriphClkInit)!=HAL_OK)err('9'),,
,HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000),,
,HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK),,
,HAL_NVIC_SetPriority(SysTick_IRQn,0,0),,
,__HAL_RCC_SYSCFG_CLK_ENABLE(),,
,__HAL_RCC_GPIOF_CLK_ENABLE(),,
,__HAL_RCC_GPIOA_CLK_ENABLE(), // tim IC + adc + dac,
,__HAL_RCC_DMA1_CLK_ENABLE(),,
,__HAL_RCC_USART1_CLK_ENABLE(),,
,__HAL_RCC_TIM2_CLK_ENABLE(),,
,__HAL_RCC_TIM3_CLK_ENABLE(), ,pin.Pin=GPIO_PIN_9,,
,pin.Mode=GPIO_MODE_AF_PP,,
,pin.Pull=GPIO_PULLUP,,
,pin.Speed=GPIO_SPEED_FREQ_HIGH,,
,pin.Alternate=GPIO_AF7_USART1,,
,HAL_GPIO_Init(GPIOA,&,pin), ,dmaUT.Instance=DMA1_Channel4,,
,dmaUT.Init.Direction=DMA_MEMORY_TO_PERIPH,,
,dmaUT.Init.PeriphInc=DMA_PINC_DISABLE,,
,dmaUT.Init.MemInc=DMA_MINC_ENABLE,,
,dmaUT.Init.PeriphDataAlignment=DMA_PDATAALIGN_BYTE,,
,dmaUT.Init.MemDataAlignment=DMA_MDATAALIGN_BYTE,,
,dmaUT.Init.Mode=DMA_NORMAL,,
,dmaUT.Init.Priority=DMA_PRIORITY_LOW,,
,if(HAL_DMA_Init(&,dmaUT)!=HAL_OK)err('a'),,
,__HAL_LINKDMA(&,uart,hdmatx,dmaUT),,
,uart.Instance=USART1,,
,uart.Init.BaudRate=115200,,
,uart.Init.WordLength=UART_WORDLENGTH_8B,,
,uart.Init.StopBits=UART_STOPBITS_1,,
,uart.Init.Parity=UART_PARITY_NONE,,
,uart.Init.Mode=UART_MODE_TX,,
,uart.Init.HwFlowCtl=UART_HWCONTROL_NONE,,
,uart.Init.OverSampling=UART_OVERSAMPLING_16,,
,uart.Init.OneBitSampling=UART_ONE_BIT_SAMPLE_DISABLE,,
,uart.AdvancedInit.AdvFeatureInit=UART_ADVFEATURE_NO_INIT,,
,if(HAL_UART_Init(&,uart)!=HAL_OK)err('b'),,
,tim.Instance=TIM3,,
,tim.Init.Period=11999,,
,tim.Init.Prescaler=999, // .25sec interupts,
,tim.Init.ClockDivision=0,,
,tim.Init.CounterMode=TIM_COUNTERMODE_UP,,
,if(HAL_TIM_Base_Init(&,tim)!=HAL_OK)err('c'),,
,if(HAL_TIM_Base_Start_IT(&,tim)!=HAL_OK)err('d'),,
,,
,pin.Pin=GPIO_PIN_2,,
,pin.Mode=GPIO_MODE_AF_PP,,
,pin.Pull=GPIO_NOPULL,,
,pin.Speed=GPIO_SPEED_FREQ_HIGH,,
,pin.Alternate=GPIO_AF1_TIM2,,
,HAL_GPIO_Init(GPIOA,&,pin),,
,timIC.Instance=TIM2,,
,timIC.Init.Prescaler=0,,
,timIC.Init.CounterMode=TIM_COUNTERMODE_UP,,
,timIC.Init.Period=0xffffffff,,
,timIC.Init.ClockDivision=TIM_CLOCKDIVISION_DIV1,,
,timIC.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE,,
,if(HAL_TIM_IC_Init(&,timIC)!=HAL_OK)err('e'),,
,smst.MasterOutputTrigger=TIM_TRGO_RESET,,
,smst.MasterSlaveMode=TIM_MASTERSLAVEMODE_DISABLE,,
,if(HAL_TIMEx_MasterConfigSynchronization(&,timIC,&,smst)!=HAL_OK)err('f'),,
,scfgIC.ICPolarity=TIM_INPUTCHANNELPOLARITY_RISING,,
,scfgIC.ICSelection=TIM_ICSELECTION_INDIRECTTI,,
,scfgIC.ICPrescaler=TIM_ICPSC_DIV1,,
,scfgIC.ICFilter=0,,
,if(HAL_TIM_IC_ConfigChannel(&,timIC,&,scfgIC,TIM_CHANNEL_4)!=HAL_OK)err('g'),,
,if(HAL_TIM_IC_Start_IT(&,timIC,TIM_CHANNEL_4)!=HAL_OK)err('h'), ,HAL_NVIC_SetPriority(TIM2_IRQn,1,1), // tim IC,
,HAL_NVIC_EnableIRQ(TIM2_IRQn),,
,HAL_NVIC_SetPriority(DMA1_Channel4_IRQn,2,2), // dma uart T,
,HAL_NVIC_EnableIRQ(DMA1_Channel4_IRQn),,
,HAL_NVIC_SetPriority(USART1_IRQn,3,3), // uart interupts,
,HAL_NVIC_EnableIRQ(USART1_IRQn),,
,HAL_NVIC_SetPriority(TIM3_IRQn,4,4), // ticking for uart,
,HAL_NVIC_EnableIRQ(TIM3_IRQn), ,while(1),}PS checked with 200MHz OSCI, nice squered signal.
Does not react to voltage source changes, current limitations or extra tantalum capacitors.
2017-02-20 4:33 PM
I don't use nor understand Cube, but can there be two functions with the same name HAL_TIM_IC_CaptureCallback() ?
Interrupts have a non-negligible latency and it takes time to enter, exit and process the interrupt. The layers in Cube won't help either. Particularities depend on used toolchain and its settings, mainly optimization settings.
I don't know what exactly __HAL_TIM_SetCounter(timIC,0); is supposed to do; but if it does what I think it does, well... I wouldn't clear or otherwise modify a timer in the ISR if I would want to measure time between edges.
Btw. it's not a good idea to transmit data through UART inside an ISR, but that does not appear to be the key problem here.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.