2024-11-30 2:08 AM
Hi
Working on a project in which I require USART1,USART2 for serial communication.(RS485.)
I am using processor STM32L053R8.
the clock used is HSI.
Timer21 interrupt is being used to measure clock period. (to test the CPU Clock).
if the communication is started continuously, TIM21 and USART1/USART2 interrupts both remain pending, hence the periodvalue is above the specified Range (above the HSI_LimitHigh) and hence the processor restartas with POR24.
can anybody help?
TIA
Ashwini
2024-11-30 2:14 AM - edited 2024-11-30 2:15 AM
Stuck in a different IRQ Handler or callback function?
Some sort of blocking delay or transmit function?
2024-11-30 2:25 AM
Or just too long execution time of the UART interrupt, so that continuous communication results in that interrupt "eat up" all the processor time?
Measure that execution time, e.g. by toggling a pin at the beginning and end of the actual ISR (Interrupt Service Routine).
JW
2024-12-08 10:15 PM
HI
Could Solve my problem.
Was stucking in DMA IRQ Handler which has same priority as TIM21.
After changing the the DMA interrupt's priority there is no reset as periodvalue is in the range
Thanks
Regards
AshwiniKool
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.