2017-10-20 1:51 PM
Hi
I am using STM32L431xx Timer3 and CC3 (compare mode ) on channel 3 and i want to trigger (ADC1 channel 1) and (DMA 1 and channel 1 ) to do collection of samples triggered on the timer edge. The timer works perfectly fine for the period I have set it work on. But I am not able to get the ADC->DMA chain working with the timer. Below are the ADC settings :
LL_ADC_SetCommonPathInternalCh(ADC1_COMMON,LL_ADC_PATH_INTERNAL_VREFINT);
LL_ADC_SetCommonClock(ADC1_COMMON,LL_ADC_CLOCK_SYNC_PCLK_DIV4); LL_ADC_SetResolution(ADC1, LL_ADC_RESOLUTION_12B); LL_ADC_SetOffset(ADC1, LL_ADC_OFFSET_1, LL_ADC_CHANNEL_1, 0x000); LL_ADC_SetOffsetState(ADC1, LL_ADC_OFFSET_1,LL_ADC_OFFSET_DISABLE); LL_ADC_SetChannelSamplingTime(ADC1,LL_ADC_CHANNEL_1, LL_ADC_SAMPLINGTIME_12CYCLES_5); LL_ADC_REG_SetDMATransfer(ADC1,LL_ADC_REG_DMA_TRANSFER_UNLIMITED); LL_ADC_REG_SetContinuousMode(ADC1, LL_ADC_REG_CONV_CONTINUOUS); LL_ADC_REG_SetTriggerSource(ADC1,LL_ADC_REG_TRIG_EXT_TIM2_TRGO); LL_ADC_Enable(ADC1);DMA settings
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
DMA_cfg.CPAR = (uint32_t)&ADC1->DR;
DMA_cfg.CMAR = (uint32_t)destAddress;//destinatoin address DMA_cfg.CNDTR = numData;//number of bytes to be trasnferredDMA1_Channel1->CCR = ( DMA_CCR_TCIE | DMA_CCR_TEIE | DMA_CCR_CIRC | DMA_CCR_HTIE| DMA_CCR_MINC | DMA_CCR_PSIZE_32BIT | DMA_CCR_MSIZE_32BIT | DMA_CCR_PL_VERY_HIGH )
DMA1_CSELR->CSELR = DMA1_CFG_CSELR; \\this value is '0' NVIC_SetPriority(DMA1_Channel1_IRQn, 0); NVIC_EnableIRQ(DMA1_Channel1_IRQn); LL_DMA_EnableChannel(DMA1,LL_DMA_CHANNEL_1);I dont see that I am able to get the ADC to trigger so that transfer happens!!!
Please help!
Regards
Bala
2017-10-20 2:38 PM
>>Please help!
Look at how I post working examples, and ask yourself how to format/present code to be worked on.
The count length for DMA is units, not bytes. The ADC->DR is 16-bit wide. I'd tinker, but see point #1
2017-10-23 12:46 PM
Hi Clive
Thanks for the suggestion:
This is what I did in the sequence below to get the TIM2 (CC on Channel 3) and that will trigger an event to start ADC1 channel 1 and I am hooking up the DMA1 channel 1 to the ADC channel
/*This function is called from main() after setting the Timer2 channel 3 to generate TRG event */
void Init_ADCwDMA( uint16_t *destAddress, uint16_t numData ){
DMA_Channel_TypeDef DMA_cfg; DMA_cfg.CPAR = (uint32_t)&ADC1->DR; DMA_cfg.CMAR = (uint32_t)destAddress; DMA_cfg.CNDTR = numData; Init_ADC(); Init_DMA(); setDMAChannel(DMA1_Channel1, &DMA_cfg);}void Init_DMA()
{
/* (1) Enable the clock of DMA1 and DMA1 */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);DMA_Channel_TypeDef DMA1_CH1_cfg = DMA1_CH1_CFG;
DMA1_Channel1->CCR = 0x3aae;//( DMA_CCR_TCIE | DMA_CCR_TEIE | DMA_CCR_CIRC | DMA_CCR_HTIE| //DMA_CCR_MINC | DMA_CCR_PSIZE_32BIT | DMA_CCR_MSIZE_32BIT | //DMA_CCR_PL_VERY_HIGH )DMA1_CSELR->CSELR = 0x0;
NVIC_SetPriority(DMA1_Channel1_IRQn, 0); NVIC_EnableIRQ(DMA1_Channel1_IRQn); LL_DMA_EnableChannel(DMA1,LL_DMA_CHANNEL_1);}/* setting DMA1 channel 1 with a config of DMA1*/
void setDMAChannel(DMA_Channel_TypeDef* channel, DMA_Channel_TypeDef *DMA_CONFIG){
channel->CCR &= ~DMA_CCR_EN; channel->CNDTR = DMA_CONFIG->CNDTR; channel->CPAR = DMA_CONFIG->CPAR; channel->CMAR = DMA_CONFIG->CMAR; channel->CCR |= DMA_CCR_EN; }void Init_ADC( void )
{ uint8_t timeout;LL_ADC_SetCommonPathInternalCh(ADC1_COMMON,LL_ADC_PATH_INTERNAL_VREFINT);//Set an internal reference voltage for ADC LL_ADC_SetCommonClock(ADC1_COMMON,LL_ADC_CLOCK_SYNC_PCLK_DIV4);//Set ADC clock to SYSCLK/.4 LL_ADC_SetResolution(ADC1, LL_ADC_RESOLUTION_12B);//12 Bit resolution LL_ADC_SetOffset(ADC1, LL_ADC_OFFSET_1, LL_ADC_CHANNEL_1, 0x000);//ADC1 channel 1 LL_ADC_SetOffsetState(ADC1, LL_ADC_OFFSET_1,LL_ADC_OFFSET_DISABLE);//Disable ADC offset LL_ADC_SetChannelSamplingTime(ADC1,LL_ADC_CHANNEL_1, LL_ADC_SAMPLINGTIME_12CYCLES_5);//set conversion time LL_ADC_REG_SetDMATransfer(ADC1,LL_ADC_REG_DMA_TRANSFER_UNLIMITED); unlimited DMA transfer LL_ADC_REG_SetContinuousMode(ADC1, LL_ADC_REG_CONV_CONTINUOUS);//continous conversion LL_ADC_REG_SetTriggerSource(ADC1,LL_ADC_REG_TRIG_EXT_TIM2_TRGO);//Generate Timer2 trigger LL_ADC_Enable(ADC1);//Enable ADC1}
void main()
{
Init_ADCwDMA( &aRcvBuf[0],160);
/ * below was timer code and the timer does work as expected as a PWM*//*The timer2 channel 3 is set in CC mode and it works good and it is tested*/
/*The code was not put out to avoid cluttering*/
/* Force update generation */
LL_TIM_GenerateEvent_UPDATE(TIM2); /* Enable output channel 3 */ LL_TIM_CC_EnableChannel(TIM2, LL_TIM_CHANNEL_CH3); LL_ADC_REG_StartConversion(ADC1);}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.