2018-12-20 9:38 AM
Can you please share me timer sample code for STM32L432G board.
I have Sensortile board and would like to interface buzzer, so I need to add timer code to get timer cb to toggle the required frequency to get the proper buzzer sound.
Also please suggest if anything is available for buzzer.
2018-12-20 9:41 AM
Timer examples which should be portable can be found in the code repository
STM32Cube_FW_L4_V1.13.0\Projects\NUCLEO-L432KC\Examples\TIM\TIM_PWMOutput
2018-12-23 11:31 AM
Note: If you use a piezo buzzer, you could use 2 TIMER PWM channels in opposite phase to double the piezo alternative voltage amplitude...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.