2022-01-11 9:23 PM
hey there
I have a STM32f030k6t6 which I wish to set a timer(TIM16 in this case) and each time timer interrupts, a GPIO pin toggles. I attach the clock configuration.
and here is my tim16 config
htim16.Instance = TIM16;
htim16.Init.Prescaler = 10;
htim16.Init.CounterMode = TIM_COUNTERMODE_UP;
htim16.Init.Period = 44236;
htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim16.Init.RepetitionCounter = 0;
htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim16) != HAL_OK)
{
Error_Handler();
}and this is start of timer
if(HAL_TIM_Base_Start_IT(&htim16)!=HAL_OK)//
{
Error_Handler();
}and finally timer interrupt and GPIO toggling
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM16)
{
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_3);
}
}now funny thing is that as I have set timer to interrupt every 10ms, but when I use oscilloscope, each timer interrupt is shown to be 4ms.
so why is that?
Solved! Go to Solution.
2022-01-12 2:50 AM
sorry all my fault...
first of all my oscilloscope was not calibrated, so false results is not unexpected...
and second is that
htim16.Init.Prescaler = 10;so this is crucial, as I forgot that Prescaler is added up by 1 in calculations.
when I wanted for example 10ms or more, this was ok(10 and 10+1 is almost the same)
nut when I wanted 1ms, this made me huge mistakes in measurments, as I expected 1ms but I forgot that in formula we use 1+1=2! which gave me 2times greater results...
anyways guys, thanks for you hints and clues
2022-01-11 10:57 PM
Output frequency is
f=(44.2368*10^6)/(10+1)/(44236+1) ' frequency in Hz
f = 90.9086799
period is
t=1/f *10^3 ' period in ms
t = 11.000049732
(if prescaler=0, frequency divided by 1, if prescaler=1 then division /2, .)
For ~10ms period prescaler must be set to 9, period to 44235
it does not explain why you observe 4ms though.
2022-01-12 12:30 AM
yeap, and more curious is this one
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM16)
{
cnt++;
if(cnt==1000)
{
cnt=0;
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_3);
}
}
}i wish to get a 1sec toggle when I count cnt each time, but same result... why is that?
2022-01-12 2:02 AM
What is "same result"? 4ms between edges?
JW
2022-01-12 2:50 AM
sorry all my fault...
first of all my oscilloscope was not calibrated, so false results is not unexpected...
and second is that
htim16.Init.Prescaler = 10;so this is crucial, as I forgot that Prescaler is added up by 1 in calculations.
when I wanted for example 10ms or more, this was ok(10 and 10+1 is almost the same)
nut when I wanted 1ms, this made me huge mistakes in measurments, as I expected 1ms but I forgot that in formula we use 1+1=2! which gave me 2times greater results...
anyways guys, thanks for you hints and clues
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.