2018-09-22 5:09 PM
I've been trying to configure the dma and pwm timer for 5 days with no luck...
There are a few things that I do not understand.
As far i know timer must be connected to a DMA to push the data.
1) In a timer there must be set a autoreload register (specified numer). What does that number means to dma? If I set autoreload to 8 it means 8 bits for dma?
2) What value should have pulse mode in PWM? Is PWM pulse set by a DMA in this case?
3) if I have uint32_t data = 0xAABBCC00 how I set that 0xAA will be send to PA0, 0xBB to PA1, 0xCC to PA2 and ignore 0x00?
4) How i can make it synchronous? Dma to gpio should be synchronous with a clock pin. I think i should use timer OC mode - am I right? If yes, pulse value of pulse should be set for OC?
I can not understand how I should configure the timer and what values for autopreload, pwm pulse, oc pulse should be set. Timers are sooo complicated :(
2018-09-22 5:29 PM
The ARR of the timer determines the period, Update is when CNT==0, the cycle after ARR==CNT
If you want the TIM to generate 8 pulses,use an Advanced TIM (TIM1/TIM8 on most parts), set the Repetition Count.
You don't want to access the TIM or GPIO 8-bit wide
To drive periodic signals onto GPIO use DMA to write the 32-bit wide GPIO->BSRR, use a DMA than is trigger from a TIM UPDATE or CCx signal of choice. Set the period to control how the APB/TIMCLK is divided down to the signal placement interval. The trigger doesn't need to be a pin, you can just set the TIM up as a timebase and use the TIMx_UP connected DMA channel/stream.
The BSRR allows you to control single or multiple pins on a bank going high or low.
You will need to make a "pattern buffer" describing the sequencing of the pins, you'd need to make 8 entries to turn the 0xAA to PA0 pattern sideways, high bits at position 0, low bits at position 16, ie 0x00000001 PA0=High, 0x00010000 PA0=Low
2018-09-24 9:33 AM
Hi @Community member ,
You may refer to "TIM_DMA" example provided under Cube package.
You may take this example as a reference to correctly configure your peripheral.
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.