2009-09-28 10:42 AM
Timer 2 CC ISR is triggered twice!?
2011-05-17 4:22 AM
Hello,
I'm trying to measure the PWM signal of a rc receiver. The falling edge of the signal triggers the tim 2 cc isr. My problem is that for some reason the ISR is triggered again only 2usec later. There are no rising nor falling edges for at least 1msec. Thanks for any help! /******************************************************************************* * Function Name : main * Description : Main program * Input : None * Output : None * Return : None *******************************************************************************/ int main(void) { #ifdef DEBUG debug(); #endif /* System clocks configuration -----------*/ RCC_Configuration(); /* NVIC configuration ---*/ NVIC_Configuration(); /* GPIO configuration */ GPIO_Configuration(); /* TIM2 Configuration */ TIM2_Configuration(); while (1) { } } /******************************************************************************* * Function Name : GPIO_Configuration * Description : Configure the used I/O ports pin * Input : None * Output : None * Return : None *******************************************************************************/ void GPIO_Configuration() { GPIO_InitTypeDef GPIO_InitStructure; /* Configure capture compare input for pwm measurement */ /* TIM2 channel 2 pin (PA.01) configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Toggle Pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); } /******************************************************************************* * Function Name : TIM2_Confgureation() * Description : * Input : None * Output : None * Return : None *******************************************************************************/ void TIM2_Configuration(void) { TIM_ICInitTypeDef TIM_ICInitStructure; //TIM_ICInitStructure.TIM_ICMode = TIM_ICMode_ICAP; TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Falling; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM2, &TIM_ICInitStructure); TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2); TIM_InternalClockConfig(TIM2); TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_TimeBaseStructure.TIM_Period = 0xFFFF; TIM_TimeBaseStructure.TIM_Prescaler = 72; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, & TIM_TimeBaseStructure); /* TIM enable counter */ TIM_Cmd(TIM2, ENABLE); /* Enable the CC2 Interrupt Request */ TIM_ITConfig(TIM2, TIM_IT_CC2, ENABLE); } /******************************************************************************* * Function Name : RCC_Configuration * Description : Configures the different system clocks. * Input : None * Output : None * Return : None *******************************************************************************/ void RCC_Configuration(void) { /* RCC system reset(for debug purpose) */ RCC_DeInit(); /* Enable HSE */ RCC_HSEConfig(RCC_HSE_ON); /* Wait till HSE is ready */ HSEStartUpStatus = RCC_WaitForHSEStartUp(); if(HSEStartUpStatus == SUCCESS) { /* Enable Prefetch Buffer */ FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); /* Flash 2 wait state */ FLASH_SetLatency(FLASH_Latency_2); /* HCLK = SYSCLK */ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* PCLK2 = HCLK */ RCC_PCLK2Config(RCC_HCLK_Div1); /* PCLK1 = HCLK/2 */ RCC_PCLK1Config(RCC_HCLK_Div2); /* PLLCLK = 8MHz * 9 = 72 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); /* Enable PLL */ RCC_PLLCmd(ENABLE); /* Wait till PLL is ready */ while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { } /* Select PLL as system clock source */ RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* Wait till PLL is used as system clock source */ while(RCC_GetSYSCLKSource() != 0x08) { } } /* Enable peripheral clocks ----------------*/ /* GPIOB Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* TIM2 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); } /******************************************************************************* * Function Name : NVIC_Configuration * Description : Configures Vector Table base location. * Input : None * Output : None * Return : None *******************************************************************************/ void NVIC_Configuration(void) { NVIC_InitTypeDef NVIC_InitStructure; #ifdef VECT_TAB_RAM /* Set the Vector Table base location at 0x20000000 */ NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0); #else /* VECT_TAB_FLASH */ /* Set the Vector Table base location at 0x08000000 */ NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0); #endif /* Enable the TIM2 global Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } [ This message was edited by: kounst on 01-09-2009 21:19 ]2011-05-17 4:22 AM
kounst,
Did you reset you CC flag in the interrupt routine like: TIM_ClearITPendingBit(TIM2, TIM_IT_CC2); ?2011-05-17 4:22 AM
yes I did.
The ISR is only called twice after each edge- so I think the problem can't be related to the interrupt flag.2011-05-17 4:22 AM
Kounst,
Did you find a reason for this as I am seeing this now?2011-05-17 4:22 AM
Hi,
yes I solved it! I figured out that if I turn off my laptop everything works fine. So I added a Schmitt Trigger. Problem solved! Regards,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.