2014-06-05 5:30 AM
Hi,
I am using TIM3(PC6 to PC9) for PWM output in STM32F215. In this I want three 50Hz PWM signals and one 8KHz signal. So I have configured PC7,PC8,PC9 as 50Hz PWM signals. For this i have assignedPrescalerValue_50 = (uint16_t) ((SystemCoreClock/2 ) / 33335) - 1;
And I have configured PC6 as 80KHz PWM signal.For this i have assignedPrescalerValue_10 = (uint16_t) ((SystemCoreClock/2 ) / 5000000) - 1;
But i am getting 8KHz in all pins. What is problem i do'nt know. Please help me asap. Below is my code void TIM_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; /* TIM3 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); /* GPIOC clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); /* GPIOC Configuration: TIM3 CH1 (PC6), TIM3 CH2 (PC7), TIM3 CH3 (PC8) and TIM3 CH4 (PC9) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Connect TIM3 pins to AF2 */ //GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_TIM3); /* Compute the prescaler value */ PrescalerValue_50 = (uint16_t) ((SystemCoreClock/2 ) / 33335) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 665; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue_50; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; } void TIM_Cong1(uint16_t Dutycycle) { GPIO_InitTypeDef GPIO_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Connect TIM3 pins to AF2 */ GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM3); PrescalerValue_10 = (uint16_t) ((SystemCoreClock/2 ) / 5000000) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 665; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue_10; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; // TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = Dutycycle; TIM_OC1Init(TIM3, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM3, ENABLE); TIM_Cmd(TIM3, ENABLE); } void PWM_Generation1(uint16_t Dutycycle) { // TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = Dutycycle; TIM_OC4Init(TIM3, &TIM_OCInitStructure); TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable); // TIM_ARRPreloadConfig(TIM3, ENABLE); TIM_Cmd(TIM3, ENABLE); } void PWM_Generation2(uint16_t Dutycycle) { // TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = Dutycycle; TIM_OC3Init(TIM3, &TIM_OCInitStructure); TIM_OC3PreloadConfig(TIM3, TIM_OCPreload_Enable); // TIM_ARRPreloadConfig(TIM3, ENABLE); TIM_Cmd(TIM3, ENABLE); } void PWM_Generation3(uint16_t Dutycycle) { // TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = Dutycycle; TIM_OC2Init(TIM3, &TIM_OCInitStructure); TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable); // TIM_ARRPreloadConfig(TIM3, ENABLE); TIM_Cmd(TIM3, ENABLE); } Regards, Thirukkannan.2014-06-05 6:28 AM
There is only one counter in each timer (and 4 capture-compare units, but they don't count), so you reprogram it to reload at a different rate when you call the other routine.
Review the timer chapter in the user manual, focus on the schematic at the beginning of the chapter. JW2014-06-05 8:59 AM
You're going about this all wrong.
Use TWO timers For 50 Hz, set the Prescaler to divide to 1 MHz, ie (SystemCoreClock / 1000000) -1, and the Period to 20000-1 (20 ms 50 Hz), you can then set the Pulse width in 1us units for the 3 channels. For 8 KHz, set the Prescaler to 0, and Period to (SystemCoreClock / 8000) -1 This would be for APB2 based timers, assuming CPU @ 120 MHz, APB2 at 60 MHz, for APB1 at 30 MHz, you'd need to use (SystemCoreClock / 2) for your TIMCLK2014-06-26 2:56 AM
Hi waclawek.jan,
Thanks for your valuable reply.2014-06-26 3:01 AM
Hi clive1,
Thanks for your quick and valuable reply. And How your calculating the Prescaler Value and Period based on frequency range.2014-06-26 4:41 AM
TIMEBASE = TIMCLK / ((PRESCALER+1) * (PERIOD+1))
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.