2010-08-18 1:09 AM
2011-05-17 5:03 AM
Seems to be OK. Of course line 'RCC->APB2ENR=' is an error.
(1 << (TIM2_IRQChannel & 0x1F)); should evaluate to 0X10000000. Does it? Is the address of TIM2_IRQhandler in the approrpiate vector location?2011-05-17 5:03 AM
2011-05-17 5:03 AM
The NVIC is the Nested Vectored Interrupt Controller and it is part of the Cortex-M3 core.
To enable an interrupt in the Cortex-M3 core, a bit in one of the the NVIC's SETENEABLE registers must be set. In the case of timer 2 on an STM32 chip, bit 28 of register SETENABLE0_31 must be set. I presume that NVIC->ISER[0] is this SETENABLE0_31 register. (We don't know for sure because we don't use your compiler.) In this case, the 0X1F mask does nothing since TIM2_IRQChannel is (or should be) 28. (1 << (TIM2_IRQChannel & 0x1F)) is therefore the same as (1 << TIM2_IRQChannel) The 0X1F mask is only required for channels that are greater than 31. If it is of interest, you can obtain the development tools that we use from here: http://www.crossware.com/trialware/21499113stm/index.htm You can use wizards to create all of the code you require and you can test it in the simulator before you run it on the hardware.2011-05-17 5:03 AM
2011-05-17 5:03 AM
I came to what was the problem its in the interrupt subroutine name ie. void Void TIM2_IRQhandler(void) which should be Void TIM2_IRQHandler(void) . now code is working fine thank you...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.